LPC1830 chirppping

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1830 chirppping

831 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shiggy on Tue Sep 03 04:30:07 MST 2013
Hi Everyone!
I am using the LPC1830 NGX Evaluation Board, using the LPCXpesso IDE.
And I am runing the USB0 in High-Speed bulk mode, by referebcing the sample source code.
I think the LPC1830 and LPCXpresso is excellent.

Q1) I want to get the source code concerning to Chirp.

If you give me any comment, it will be very help for me.

Shiggy
0 项奖励
回复
2 回复数

822 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shiggy on Mon Sep 09 02:13:13 MST 2013
Hi rocketdawg-san

Thanks your answer.

>you need to change the USB descriptor to say the the max packet size is 512 bytes not 256.
512 is for High Speed.
<--- I have already tried, and have successed.

Shiggy


0 项奖励
回复

822 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Thu Sep 05 14:57:21 MST 2013
USB chirps are under hardware control, not software.
I read your other post.

you need to change the USB descriptor to say the the max packet size is 512 bytes not 256.
512 is for High Speed.
0 项奖励
回复