LPC1788 not recognized on LPCXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 not recognized on LPCXpresso

1,517 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by enzolazo on Fri May 23 18:14:07 MST 2014
Hello,

I am new to LPC boards and LPCXpresso. I am trying to program a simple example project to the LPC1788-32 Developer's kit board. I am following this tutorial: http://mc2.unl.edu/2013/10/04/lpcxpresso-hello-world-and-breadboard-led-blinking/#fn1-154

Unfortunately, I am getting this error message:

[img]http://s16.postimg.org/b6gu2iwb5/Screen_Shot_2014_05_23_at_9_45_33_PM.png[/img]

I have tried both USB ports of my Macbook Air and also an external 5V power source.
Additionally, as I have not found the information about which micro-USB board port I should connect to power/program the board, I have tried all possible combinations on the three micro-USB board ports (see image bellow)

[img]http://s16.postimg.org/whee6sefl/IMG_9673.jpg[/img]

I have no idea why it is not working. Is there need for installing any drivers? If not, what could I do to get this to work?

Thank you all,
Enzo
0 项奖励
回复
5 回复数

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat May 24 02:34:00 MST 2014
How about reading the LPCXpresso manual?
http://www.lpcware.com/content/nxpfile/lpcxpresso-ide-v7-user-guide
0 项奖励
回复

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri May 23 23:55:34 MST 2014
This boards are available since 2011 and this manual isn't very up-to-date....

Chapter 5.4 is talking about SWD interface.

What you need to use LPCXpresso as Debugger is a LPC-link or LPC-link2 and a ribbon cable for J7  :)

Link2:
http://www.embeddedartists.com/products/lpcxpresso/lpclink2.php


Ribbon cable:
http://www.embeddedartists.com/products/acc/acc_idc_10.php
0 项奖励
回复

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by enzolazo on Fri May 23 23:45:26 MST 2014
Yes, I have took a time and read about how to program the board. But unfortunately, the User Manual only shows how to program using Flash Magic tool. And I do not see it informing about LPC-link. What would be that? Is it necessary for the programming step?
0 项奖励
回复

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Fri May 23 23:28:01 MST 2014

Quote: enzolazo
I have no idea why it is not working.



Which LPC-link are you using and how did you connect it?

Did you read the User Manual?

http://www.embeddedartists.com/products/oem/lpc1788_oem.php

Quote:

4.23 SP13: Power Supply

The power supply on the board is straight forward. There are three powering sources:
1. +5V DC via 2.1mm power jack (J24). Center pin positive. There is also an alternative connector (J23) for this powering option.

2. USB powering via the USB-to-UART Bridge connector (J25).

3. +5V DC power form the PoE (Power-over-Ethernet) connector (J12)

0 项奖励
回复

1,472 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by enzolazo on Fri May 23 22:25:50 MST 2014
I could now find which micro-USB is used to power/program the board. In fact, I downloaded Flash Magic and I was able to program the LCP1788 board. But I still can't program the board using the LCPXpresso software. Any idea?
0 项奖励
回复