LPC1788 Clock disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 Clock disabled

791 次查看
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by Thucydides on Sat Feb 11 00:28:43 MST 2012
Hello,

When I was writing a code for LPC1788, I made a big mistake.
As for setting of the CPU Clock Selection register (CCLKSEL - 0x400F C104), I've designated 0 and soon I noticed a explanation on the document.

"The divider is turned off., no clock will be provided to the CPU. This setting
should typically not be used, the CPU will be halted and a reset will be required to restore operation."

At LPC1769's CCLSEL 0 means just divide 1 but at LPC1788 CPU clock stops!
After download it, naturally any debug or run became disabled via LPCXpresso IDE and flashmagic.
Error on the LPCXpresso was
"02:Failed on connect:Em(01).Cannot find selected MEM-AP(check target  power):"

How could I turn on the clock of the lPC1788??
If there are anyone who know the solution, please show me how to escape from the situation.

Thanks,
Thucydides

http://knowledgebase.nxp.com/member.php?u=1317

0 项奖励
回复
1 回复

680 次查看
lpcware
NXP Employee
NXP Employee

Content originally posted in LPCWare by TheFallGuy on Sat Feb 11 02:04:00 MST 2012
Read the FAQ?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip

You can save yourself a lot of time by searching the the forum or support articles before posting. Information on how to search is in the sticky post at the top of the forum.

0 项奖励
回复