LPC1769 simple circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769 simple circuit

1,603 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gkdavidse on Wed Jul 03 14:49:40 MST 2013
Hi

I am fairly new to ARMS and would like to experiment with the LPC1769 as a standalone much in a custom circuit. I've played with the lpcXpresso and know how the IDE etc works.

Does anyone have a schematic for a simple lpc1769 with an led connected (including crystal etc) to it as well as circuitry to enable programming with the link board from the xpresso?

Thanks :)
0 项奖励
回复
6 回复数

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gkdavidse on Thu Jul 04 01:22:54 MST 2013
thanks ;-)
0 项奖励
回复

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jul 03 15:37:44 MST 2013

Quote: gkdavidse
Ok cool. So I just need power, crystal and the appropriate connections to the link programmer?



+ISP Button +Reset Button +UART Connector :)
0 项奖励
回复

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gkdavidse on Wed Jul 03 15:22:09 MST 2013
Ok cool. So I just need power, crystal and the appropriate connections to the link programmer?
0 项奖励
回复

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jul 03 15:14:21 MST 2013

Quote: gkdavidse
It is, but I want to build my own circuit using the lpc1769. I am no pro, so help would be appreciated.



And what's wrong with starting with target board schematic?

Or ask Google?

'LPC1768 schematic' throws 37200 results here, like:

http://www.google.de/imgres?imgurl=http://dangerousprototypes.com/docs/images/thumb/b/b1/Cct-LPC1768...
0 项奖励
回复

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gkdavidse on Wed Jul 03 15:08:57 MST 2013
It is, but I want to build my own circuit using the lpc1769. I am no pro, so help would be appreciated.
0 项奖励
回复

1,553 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Jul 03 14:59:07 MST 2013
Isn't LPCXpresso1769 target board simple enough?
0 项奖励
回复