LPC1769 UART baudrate 1Mb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1769 UART baudrate 1Mb

1,093件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DiamondS on Mon Apr 16 23:55:16 MST 2012
Is it possible to run UART in 1 Mb?

What i'm trying to do is communicate with Dynamixel Servo AX-12.
And i realized that something wrong with baud rate.
0 件の賞賛
返信
2 返答(返信)

1,065件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DiamondS on Wed Apr 18 06:45:55 MST 2012
Thanks. It helped.
Using a 96 MHz clock is not working, so i use 64MHz and everyhing is fine with 1Mb baudrate.
0 件の賞賛
返信

1,065件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gbm on Tue Apr 17 01:18:32 MST 2012
Yes, but your system clock must be a multiple of 16 MHz (otherwise you will need to use fractional divider on UART)  - 96 MHz should be the right choice.
0 件の賞賛
返信