LPC1769 EasyVr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 EasyVr

1,109 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by iantycoon on Wed Sep 19 01:54:33 MST 2012
Hi guys,

I'm currently trying to interface my LPC1769 with an EasyVR module.

The EasyVR has 4 pins TX, RX, VCC and GND. I've connect VCC and GND to pins 28 and 1 respectively. As for TX and RX, I've connected them to RXD1 (p0.15) and TXD1 (p0.16) respectively.

May I know if such a connection for TX and RX is correct?

Many thanks,
Ian Loke
0 Kudos
Reply
3 Replies

1,101 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by iantycoon on Wed Sep 19 08:54:50 MST 2012
May I know if anyone has implemented EasyVR before?
0 Kudos
Reply

1,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by iantycoon on Wed Sep 19 05:58:22 MST 2012
Thanks for the correction Zero!
0 Kudos
Reply

1,100 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Sep 19 04:50:34 MST 2012
No , UM10360 ;)

P0[15] = TXD1
P0[16] = RXD1
0 Kudos
Reply