Content originally posted in LPCWare by jlara on Wed Mar 30 19:57:53 MST 2011
Hello Zero, NXP,
Can you please let me know if you agree with the following BTR calculations?
PLL = 72MHz
CAN Baudrate: 500KHz
Tq = 18
TSEG1 = 14
TSEG2 = 3
SJW = 3
BRP = 1
TSEG1 = 14, TSEG2 = 3, BRP = 2
CANxBTR = 0x003EC001 Is this correct? If not, can you be so kind as to point to the error and why it is incorrect.
If anyone from NXP, CodeRed, or EA is moderating this forum, any input would be appreciated, as well as any useful links.
Zero, what CAN tool do you use? The tool you posted a while ago of a CAN message looks nice. It appears you have a scope which can decode a CAN message ID, data bytes, etc. I am in the market for a good tool if it is affordable.