LPC1769 CAN bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769 CAN bus

1,087 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PRomain on Thu Aug 11 07:54:33 MST 2011
Hello,
I have a board with an LPC1769, I created a small side mounting a transceiver to create a connection to the BUS CAN2, but I have problems in creating the program of communication between the board and a sensor (equipped with a CAN bus). If there are people who have successfully completed a program that works to tipe application,  I'm interested to fit my system.
Thank you.
Sorry for my English, I'm French ...:(
0 项奖励
回复
3 回复数

1,055 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Aug 28 09:08:45 MST 2011

Quote: Ajay
Has anyone tried lpc17_CAN__LedControl with CMSIS v2.



Yes :)
0 项奖励
回复

1,055 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ajay on Sun Aug 28 08:55:43 MST 2011
Hello,

Has anyone tried lpc17_CAN__LedControl with CMSIS v2.  I tried it with v1.3 and got very busy at wor?  I would like to get back on it but curious if v2 will give me trouble.

Thanks!
0 项奖励
回复

1,055 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Aug 11 08:14:24 MST 2011
Bonjour,

what about CAN LedControl example ?

http://support.code-red-tech.com/CodeRedWiki/NXPDriverLibraries?highlight=%28lpc17\_CAN\_\_LedContro...

Note: change files of #39: http://knowledgebase.nxp.com/showthread.php?p=10766#post10766

Sorry for my french, I'm german...
0 项奖励
回复