LPC1768 with 4:3 display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 with 4:3 display

1,581 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Wed Jul 27 02:39:47 MST 2011
Hi!
I would drive a display 4,3" 480 x 272 (RGB interface)with LPC1768 ; is there any example of it?
I know that LPC1788 has integrated lcd driver, but if I want 1768 , can I drive it?

Thanks
0 Kudos
Reply
5 Replies

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Thu Sep 01 07:57:45 MST 2011
Embedded Artists has a 480x272 4.3"LCD board for their new LPC1788 ... if you purchase it you can (I believe) access some initialisation and sample code for it.  Check if it is the same controller or model, though, since there are a number of variations on these displays ... 16-bit, 24-bit, etc.  All the work on the SW side is the init sequence and setting up the SDRAM for the framebuffer if the LCD doesn't have a built in controller ... the only real problem on the HW side is usually setting up the backlight with a stable supply if it's a wierd voltage.
0 Kudos
Reply

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mhjerde on Wed Aug 31 07:54:49 MST 2011
Your main challenge is to initialize the display properly. If you don't have example code for your particular display, you need to get the init sequence from the controller chip data sheet.
0 Kudos
Reply

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giamby3000 on Wed Aug 31 07:11:52 MST 2011

Quote: NXP_Europe
Hello giamby3000,

The MCB1700 of Keil is equipped with an LCD screen (320 * 240) ... you may get new ideas by reading their information.



Thank you very much, but MCB1700 drive LCD in SPI mode...
0 Kudos
Reply

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Thu Jul 28 05:03:41 MST 2011
As NXP mentionned, any SW example should get you 90% towards your goal since the code is mostly generic to any TFT LCD.  Afterwards, you just need to adjust the timing for your specific display and wiring it up accordingly (supplying the appropriate voltage for the backlight).
0 Kudos
Reply

1,460 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Wed Jul 27 06:44:39 MST 2011
Hello giamby3000,

The MCB1700 of Keil is equipped with an LCD screen (320 * 240) ... you may get new ideas by reading their information.
0 Kudos
Reply