LPC1768 SSP1 configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1768 SSP1 configuration

1,239 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Thu Jan 03 23:54:38 MST 2013
I have two question on SSP1 of LPC1768

1. We have configured SSP1 as TI SSI for receiving 16 bits of data. We have connected Sclk pin to Clock of salve and MISO pin to Data pin of Slave.We have generated clock to receive data from our slave. If i send the clock then SPDR value is getting updated but RNE bit is not set thus we are not able to read SPDr value. If we send the clock again my SPDR is always 0.

2. Can we read 18 bit data from the SSP1 which is configured as TI SSI with DSS as 9 bit and receiving SPDR value twice.

Code:

int main()
{
          int j;

           SystemInit();

           SSP1Init();
           LPC_SSP1->DR=0x0000;
           SSPSend(1,0x0000,16);


          while(1)
          {


     }
 }

void SSP1Init( void )
{
    uint8_t i, Dummy=Dummy;
    LPC_SC->PCONP |= (0x1<<10);/* Enable AHB clock to the SSP1. */
    LPC_SC->PCLKSEL0 &= ~(0x3<<20);
     /* P0.6~0.9 as SSP1 */
    LPC_PINCON->PINSEL0 &= ~((0x3<<12)|(0x3<<16)|(0x3<<18));
    LPC_PINCON->PINSEL0 |= ((0x2<<12)|(0x2<<16)|(0x2<<18));

    /* Set DSS data to 8-bit, Frame format SPI, CPOL = 0, CPHA = 0, and SCR is 15 */
     LPC_SSP1->CR0 = 0x075F;
     /* SSPCPSR clock prescale register, master mode, minimum divisor is 0x02 */
     LPC_SSP1->CPSR = 0x2;
     for ( i = 0; i < FIFOSIZE; i++ )
     {
        Dummy = LPC_SSP1->DR;                /* clear the RxFIFO */
     }
   NVIC_EnableIRQ(SSP1_IRQn); /* Enable the SSP Interrupt */

   LPC_SSP1->CR1 = SSPCR1_SSE;/* Master mode *//* Device select as master, SSP Enabled */

  /* Set SSPINMS registers to enable interrupts */
  /* enable all error related interrupts */
  LPC_SSP1->IMSC = SSPIMSC_RORIM | SSPIMSC_RTIM;
  return;
}

void SSPSend( uint32_t portnum, uint16_t buf)
{
  uint32_t i;
  uint16_t Dummy = Dummy,receive[9];
      if ( portnum == 1 )
        {
          /* Move on only if NOT busy and TX FIFO not full. */
          while ( (LPC_SSP1->SR & (SSPSR_TNF|SSPSR_BSY)) != SSPSR_TNF );
          LPC_SSP1->DR = buf;
          //buf++;
    #if !LOOPBACK_MODE
          while ( (LPC_SSP1->SR & (SSPSR_BSY|SSPSR_RNE)) != SSPSR_RNE );

          LPC_SSP1->DR=0x0000;
          receive[0] = LPC_SSP1->DR;
#else
          /* Wait until the Busy bit is cleared. */
          while ( LPC_SSP1->SR & SSPSR_BSY );
#endif
    }

  return;
}
0 项奖励
回复
0 回复数