LPC1768 FreeRTOS example 7.x with CMSIS 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768 FreeRTOS example 7.x with CMSIS 2.0

1,226件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tridentsx on Wed Oct 05 21:27:16 MST 2011
Are there any FreeRTOS 7.x examples for LPC1768 or LPC1769 using CMSIS 2.0 available?

I have tried searching and I couldn't find any, there used to be a FreeRTOS example using CMSIS 1.3 in old versions of LPCExpresso but its not included anymore in latest version 4.1

Regards /// Carl
0 件の賞賛
返信
2 返答(返信)

1,108件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tridentsx on Mon Oct 10 00:12:45 MST 2011

Quote: tridentsx
No need to reply I have figured it out.



I still would like to see an example of freertos and CMSIS working together, I am doubtful about the h/w init when using both. Can I call the CMSIS inits from freertos, or does freertos use their own inits in the portable part ?

The reason I want to use CMSIS is that the examples of uart drivers for LPC1769 that  I have found all uses variable SystemCoreClock which is part of CMSIS framework.

Maybe there are other examples of uart usage for freertos and lpc1769?
0 件の賞賛
返信

1,108件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tridentsx on Fri Oct 07 08:04:02 MST 2011
No need to reply I have figured it out.
0 件の賞賛
返信