LPC1765 build issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1765 build issue

749件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pnataraj on Mon Oct 29 02:54:27 MST 2012
We have a LPC1769(with JTAG interface) and a LPC1765 (no JTAG interface).

We tried two different projects for LPC1769:
i)UART echo code (NXP's sample)
ii)Simple LED blinker.
Both of them worked fine.
We used LPCXpresso IDE to build our projects.

To test on our 1765 board,we changed the MCU options to 1765 and  rebuilt; created a hex out of the axf file  (http://support.code-red-tech.com/CodeRedWiki/PostProcessApp) and  flashed the 1765 board using "FlashMagic".
The change din't work.

Are there specific build options for LPC1765? or are we missing anything?

Note: Hex flash for LPC1769 works!!
0 件の賞賛
返信
1 返信

739件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by daniel.widyanto on Mon Oct 29 19:57:35 MST 2012
Try this: http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget
0 件の賞賛
返信