LPC1347/45 ADC Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1347/45 ADC Questions

811件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ub3r on Wed Oct 31 07:36:22 MST 2012
Hi Guys,

Ive been using the LPC1343 and for the ADC i just used the drivers given to us in the example projects.

Ive now moved onto the LPC1347 (as the LPC1343 is been discontinued) and wondering if there is an existing driver/example available before i port the 1343 driver over.

I've searched but didn't find anything. :(

cheers
0 件の賞賛
返信
2 返答(返信)

790件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cfb on Mon Dec 03 14:39:16 MST 2012
[FONT=Arial][SIZE=2]See the discussion "[/SIZE][/FONT][FONT=Arial][SIZE=2]Examples for LPC1347":[/SIZE][/FONT]

http://knowledgebase.nxp.com/showthread.php?t=3701


0 件の賞賛
返信

790件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pboogaards on Mon Dec 03 08:13:42 MST 2012
Please note that the LPC1342 and LPC1343 are not being discontinued, so you can continue to use these devices in new designs.
Regards
Paul
0 件の賞賛
返信