LPC1343 Baseboard Sample Applications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1343 Baseboard Sample Applications

1,628 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jcatania on Wed Jul 14 21:54:26 MST 2010
I am currently using the LPC1343 debugger with the LPCXpresso base board. The manual that comes with it references a zip file with sample applications that are available for download from the Embedded Artists support site (the given zip file is "lpc1343_base_board_100125.zip"). 

After browsing the EA site, googling around, and looking through the forums, I have not found the zip file.  The closest thing I've found is the example applications for the LPC13XX here: http://ics.nxp.com/support/lpcxpresso/#Examples, which includes sample applications for the different debuggers.   This file does contain deployable sample applications.  However, I am very interested in the "demo" application that the manual describes, which is not included in that particular download.  The demo application that I am interested in changes the LEDs based on teh accelerometer, the joystick draws a line on the OLED display, the rotary switch changes the digits on the 7-segment display, the SW3 button plays a melody, and the pot will turn on/off the RGB LED's.  Is the demo application available elsewhere? Or is it no longer supported?
0 Kudos
Reply
4 Replies

1,457 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wilfriedvoss on Wed Jul 02 06:17:26 MST 2014
For those who find this entry through web search: The previously hyperlink to the sample code does not work anymore...
Let's try this one: http://www.embeddedartists.com/support/xpr/base (login required).
0 Kudos
Reply

1,457 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jcatania on Thu Jul 15 17:37:24 MST 2010
Thanks!  My baseboard is alive!
0 Kudos
Reply

1,457 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Thu Jul 15 10:56:44 MST 2010
As also written by CodeRedSupport, you need to register your board with EmbeddedArtists. In the box with the baseboard you will find a paper with a label attached to it containing the product serial number.
Create a login on the EA support page and register your serial number.

Only after this you will be able to reach the Product support - LPCXpresso Base Board page. That page contains the manual, schematics, data sheets of the ICs used and the sample code you are looking for.

Regards,

Rob
0 Kudos
Reply

1,457 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Jul 15 00:13:45 MST 2010
The baseboard related example code is available from the Embedded Artists baseboard support page :)

http://www.embeddedartists.com/support/xpr/base/index.php
[login required]

I believe that you will need to register your board with Embedded Artists in order to get to this page. For more details see:

http://www.embeddedartists.com/support/

Regards,
CodeRedSupport
0 Kudos
Reply