LPC1313 Clockwire on Low

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1313 Clockwire on Low

677 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by m.Harms on Thu May 13 03:14:41 MST 2010
Helle at all,

I have a application with the LPC 1313 and 1113. After the first programming I can´t reprogramm the device.
The programmer have an error request. The SWCLK pin is low when I connect the programmer to the board.

In the application I have the reset pin set as IO Pin and disable all Pullup and Pulldown Resitors.

In the user manuel I have found a note that not allowed is to use the reset pin as IO pin.

Can anybody help me with this problem?
0 项奖励
回复
1 回复

669 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by domen on Sat May 22 11:03:46 MST 2010
Manually pull-up the Reset pin with ~10k resistor?

Still, I find this a bit weird, on power fail IO pin settings should reset, no?
0 项奖励
回复