LPC1226 GPREG1 & GPREG2 reset values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1226 GPREG1 & GPREG2 reset values

712件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Mon Dec 12 09:10:15 MST 2011
Hi,
Hi,
I am looking to use PMU GPREG1 and GPREG2 in my design. Looking in the  manual it suggests these should reset to 0x00000000 at power up. I am finding at  power up that via the debugger that  GPREG1 and GPREG2 are both being set to Ox292E or 0x293A  I have tried a complete power down and checked that the power rails have fallen to 10mV or less.

Any suggestions?

Thanks
0 件の賞賛
返信
1 返信

703件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Mon Dec 12 09:25:32 MST 2011
Problem solved,
the debugger lets the program run before entering the debug state. In this instance it is required to erase flash and then enter the debugger.This ensures that the program hasn't been able to run before debugging.
0 件の賞賛
返信