LPC11U24FBD64 pinout support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11U24FBD64 pinout support

1,085 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by keith on Mon Apr 02 08:58:38 MST 2012
Hello,

In Xpresso it appears that when selecting the LPC11U24/401 MCU, only the LPC11U24FBD48/401 is supported.  Any chance we can get an updated XML file to support the LPC11U24FBD64/401?

Best regards,
Keith
0 Kudos
Reply
3 Replies

1,073 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun Apr 15 03:47:45 MST 2012
LPCXpresso does not distinguish between different pin package versions of the same part. From the tools point of view we allow selection of LPC11U24/401 - which is intended to cover LPC11U24FHN33/401, LPC11U24FBD48/401 and LPC11U24FBD64/401.

However I agree the IOCON definitions should provide access to the 64 pin variant settings. We'll look into what can be done here for a future release.

Regards,
CodeRedSupport
0 Kudos
Reply

1,073 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by keith on Wed Apr 11 09:11:06 MST 2012
When debugging and viewing the IOCON register in the memory window, the 64 pin part should offer a number of options for routing the UART Rx pin (e.g. [FONT=&quot]PIO1_17) not available on the 48 pin package[/FONT]. When working with the 64 pin part, however, we've only seen the UART Rx pin options for the 48 pin version.

How are the different packages selected? Is the package determined at download time when the Chip ID is read?

Thanks!
0 Kudos
Reply

1,073 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 02 12:49:41 MST 2012
The LPC11U24/401 part provided in LPCXpresso is intended to cover LPC11U24FHN33/401,
LPC11U24FBD48/401 and LPC11U24FBD64/401.

Can you clarify what you think is missing?

Regards,
CodeRedSupport
0 Kudos
Reply