LPC11C24 Problems with the CAN Tx Callback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11C24 Problems with the CAN Tx Callback

651 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Abandoner on Wed Aug 08 14:07:07 MST 2012
Hi,
I am using the LPC11C24 with the Xpresso Board and also in custom designs. My problem is sending CAN Messages at a "short" period like 10 to 50 ms. It is causing a halt (All my CAN_TX Buffers are busy) after about 100 to 200 Messages and the CAN_Tx Callback  is not called anymore.

[EDIT] Solved : I used an bitwise "&" instead of "&&" in an if statement
0 Kudos
Reply
1 Reply

601 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Aug 08 14:26:29 MST 2012

Quote: Abandoner
Does anyone have any suggestions?



Yes :)

Reduce you project as far as you can and post it. That's easier than answering thousand questions :eek:
0 Kudos
Reply