[LPC1114 Motor Ctrl Kit Question]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LPC1114 Motor Ctrl Kit Question]

767 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by persecution on Tue May 21 03:10:07 MST 2013
Dear all:

I am the new one to LPC-series. Now, my mission is to use LPC1114 and Motor control kit(produced by embedded arists) to control BLDC motor. However, my boss also want me to control LPC1114 by PC. In other words, I need to send command from PC to LPC1114, and then use LPC1114 to control BLDC motor. Is that possible? If not, what kind of combination can do it?

Thanks.
0 Kudos
Reply
1 Reply

761 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue May 21 03:28:40 MST 2013
LPC1114 has an UART and AFAIK 'LPCXpresso Motor Control Kit' has an UART-to-USB interface. That's an easy way to send commands and receive messages.
0 Kudos
Reply