LPC1114 Crystal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1114 Crystal

1,524 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JAAA on Thu Jun 30 06:28:24 MST 2011
Hello

I have a lpc1114 connected with 25 MHz external cyrstal. The lpc1114 MCU internal crystal is 12 MHz. Through the pin 3 (RESET), pin 29 (SWCLK) and pin 39 (SWDIO), I connect the MCU to LPC - Link. My question is why can not debug? It is possible?
0 项奖励
回复
4 回复数

1,462 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kendwyer on Thu Jun 30 16:21:33 MST 2011
The LPC1114 will always boot from IRC regardless of the external Xtal connected - assuming you are not driving the Xtal pins beyond ~1.8v.

If it is a non programmed part it should be still possible to connect with SWD.
0 项奖励
回复

1,462 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jun 30 09:25:42 MST 2011

Quote: JSalisbury
Note to NXP, it would be usefull if the blinky project checked for unlocked PLL before switching to the PLL output!



Isn't

  LPC_SYSCON->SYSPLLCTRL    = SYSPLLCTRL_Val;
  LPC_SYSCON->PDRUNCFG     &= ~(1 << 7);          /* Power-up SYSPLL          */
  while (!(LPC_SYSCON->SYSPLLSTAT & 0x01));          /* Wait Until PLL Locked    */
in System_LPC11xx.c doing that :confused:
0 项奖励
回复

1,462 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JSalisbury on Thu Jun 30 09:05:45 MST 2011
The problem is that the device could be trying to start up against the external crystal, and the device is unstable against the unlocked PLL. To fix the problem use Flashmagic and a USB to TTL uart. This will let you use flash magic to reprogram the device.

Note to NXP, it would be usefull if the blinky project checked for unlocked PLL before switching to the PLL output!
0 项奖励
回复

1,462 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jun 30 06:42:53 MST 2011

Quote: JAAA
...is why can not debug? It is possible?



Don't know why it's not working. It's possible :) and therefore I would guess you have a hardware problem or did forget to change PLL settings :confused:
0 项奖励
回复