LPC xpresso P0.10 CLK problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC xpresso P0.10 CLK problem

948件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Electron on Wed Mar 20 07:13:04 MST 2013
hello,
I am using lpc xpresso (LPC1114) I have two test boards, and both were working fine. and then I use one of my debug board (recently solder) to burn program in them..
and ow Then I am facing a very rare problem,,,

When I burn Program I2C or SPI (ssp), I am getting clock on port P0.10,,., I don't understand what wrong with it.,.

In i2c program , the clock should be on, SCL.,. nut instead of this the clock is generating on P0.10 :(

Also in SSP the clock is coming from P0.10
Plz help. Is there any hardware setting changed?? I really dont understand :(:(
0 件の賞賛
返信
2 返答(返信)

926件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Electron on Wed Mar 20 08:11:27 MST 2013
No :(
sorry for my grammar

after the program is burned from my new LPC-Link, there is no clock on SCL for I2C and SCK for SSP.
but before burning from other LPC-Link both examples LPC1114 SSP and I2C worked.

But now examples are working... Blinky,uart,adc still working but no SPI and I2C why,.,,
0 件の賞賛
返信

926件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 20 07:20:59 MST 2013

Quote: Electron
When I burn Program I2C or SPI (ssp), I am getting clock on port P0.10,,., I don't understand what wrong with it.,.




Default function (see IOCON_SWCLK_PIO0_10 register) for PIO0_10 is SWCLK :p:p

That's your Debug Connection (SWD) Clock ;)

http://www.support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections
0 件の賞賛
返信