LPC Variants Support in LPC Expresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Variants Support in LPC Expresso IDE

650 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vineetrvce on Fri Jun 08 22:36:46 MST 2012
Hello All,
   I am using the LPC Expresso IDE from Code Red. I am able to work with LPC1114/302 ICs.

But the IDE does not list the followinf targets:

LPC1115
LPC1114/323
LPC1114/333
LPC1114/302

and so on.

So how can I use these IC's to develop. So I need to change settings in the IDE to support more targets? as Code Red IDE claims that we can debug upto 128kb of source code?

Regards.
Vineet.
0 Kudos
Reply
1 Reply

642 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Jun 09 01:12:39 MST 2012
The parts you list are all supported in v4.2.3 of LPCXpresso.

You can develop and debug code up to 128k - but only if the chip you are using supports that size.... The largest LPC11xx part contains only 64k of flash (the LPC1115).
0 Kudos
Reply