LPC-Link2 as an evaluation board for LPC4370

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link2 as an evaluation board for LPC4370

1,234 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suhel on Sat Sep 20 00:23:16 MST 2014
Hi,

I am new to LPC platform and i intent to use LPC4370 because of it's high data capture capabilities (HSADC).

One basic doubt,

when using LPC-Link2 as target board of LPC4370 do i need a second LPC-Link2 board for debugging??

when using the LPC-Link2 as evaluation board, does it support debugging using LPCEpresso??


Please respond at the earliest.


Regards,
Suhel
0 Kudos
Reply
4 Replies

1,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suhel on Mon Sep 22 21:54:48 MST 2014
Thanks for your timely response.

Regards,
Suhel
0 Kudos
Reply

1,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Sep 22 07:04:47 MST 2014
Yes
0 Kudos
Reply

1,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by suhel on Mon Sep 22 06:38:45 MST 2014
Let me summarize my understanding here,

if u want to use LPC-LINK2 for evaluation of LPC4370 (target), then you need to use one more LPC-LINK2 as a debug probe.

So essentially you need to have two LPC-LINK2 boards one as debug probe and other one as target.

You cannot debug with a single LPC-LINK2 board.

Correct?
0 Kudos
Reply

1,130 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sat Sep 20 00:52:00 MST 2014
The answer to both questions is Yes.

See also this FAQ:
http://www.lpcware.com/content/faq/lpcxpresso/using-lpclink2-as-lpc4370-eval
0 Kudos
Reply