LPC-Link2 - How to switch the JTAG mode ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC-Link2 - How to switch the JTAG mode ?

1,852 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Badman on Fri Jan 17 00:33:38 MST 2014
Hello,

I have connected JTAG connector J6 in LPC-Link2. When I program the target system is a message that is in the SWD.

Ni: LPCXpresso RedlinkMulti Driver v6.0 (Nov 20 2013 07:01:29 - crt_emu_cm_redlink.exe build 252) 
Pc: (  0) Reading remote configuration 
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/LPC1768.xml 

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/NXP_directory.xml 

Nc: Found generic directory XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/crt_directory.xml 

Pc: (  5) Remote configuration complete 
Pc: ( 30) Emulator Connected 
Pc: ( 40) Debug Halt 
Pc: ( 50) CPU ID 
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. CpuID: 410FC230. Info: (null) 
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled. 
Nc: Loaded LPC175x_6x_512.cfx: LPC175x_6x (512K) Apr 22 2013 12:14:31  On-chip Flash Memory 

Pc: ( 65) Chip Setup Complete 
Nt: Connected: was_reset=true. was_stopped=false 
Cr:v LPCXpresso Free License - Download limit is 256K 
Pc: ( 70) License Check Complete 
Nt: Loading ELF file LCD.axf' at location 00000000 
Nt: Writing 64268 bytes to 0000 in Flash (assumed clock: unknown) 
Pb: 1 of 2 (  0) Writing pages 0-7 at 0x00000000 with 32768 bytes 
Ps: (  0) Page  0 at 00000000 
Ps: (  0) Page  0 at 00000000: 4096 bytes 
Ps: ( 12) Page  1 at 00001000: 4096 bytes 
Ps: ( 25) Page  2 at 00002000: 4096 bytes 
Ps: ( 37) Page  3 at 00003000: 4096 bytes 
Ps: ( 50) Page  4 at 00004000: 4096 bytes 
Ps: ( 62) Page  5 at 00005000: 4096 bytes 
Ps: ( 75) Page  6 at 00006000: 4096 bytes 
Ps: ( 87) Page  7 at 00007000: 4096 bytes 
Nt: Erased/Wrote page  0-7 with 32768 bytes in 5996msec 
Pb: 2 of 2 ( 50) Writing pages 8-15 at 0x00008000 with 31500 bytes 
Ps: (  0) Page  8 at 00008000 
Ps: (  0) Page  8 at 00008000: 4096 bytes 
Ps: ( 13) Page  9 at 00009000: 4096 bytes 
Ps: ( 26) Page 10 at 0000A000: 4096 bytes 
Ps: ( 39) Page 11 at 0000B000: 4096 bytes 
Ps: ( 52) Page 12 at 0000C000: 4096 bytes 
Ps: ( 65) Page 13 at 0000D000: 4096 bytes 
Ps: ( 78) Page 14 at 0000E000: 4096 bytes 
Ps: ( 91) Page 15 at 0000F000: 2828 bytes 
Nt: Erased/Wrote page  8-15 with 31500 bytes in 5622msec 
Pb: (100) Finished writing Flash successfully. 
Nt: Flash write Done 


How to switch the JTAG mode ?
0 项奖励
回复
3 回复数

1,686 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jan 17 14:06:44 MST 2014
There is a bug in what is reported by the debug driver. It is reporting swd regardless of what type of connection. This is fixed in the next release.

If jtag is correctly selected in the debug configuration, you will be prompted to select a core.
0 项奖励
回复

1,686 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Badman on Fri Jan 17 13:44:14 MST 2014
Changed as shown in the link on the JTAG, but still program and debugger in SWD.

LPCXpresso RedlinkMulti Driver v6.0 (Nov 20 2013 07:01:29 - crt_emu_cm_redlink build 252)
Looked for chip XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/LPC4088.xml
Looked for vendor directory XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/NXP_directory.xml
Found generic directory XML file in C:/nxp/LPCXpresso_6.1.2_177/lpcxpresso/bin/crt_directory.xml
(  5) Remote configuration complete
Emu(0): Conn&Reset. DpID: 4BA00477. CpuID: 410FC240. Info: (null)
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Loaded LPC177x_8x_407x_8x_512.cfx: LPC177x_8x_407x_8x (512K) Apr 22 2013 12:14:33  On-chip Flash Memory
Connected: was_reset=false. was_stopped=true
v LPCXpresso Free License - Download limit is 256K
Writing 7160 bytes to 0000 in Flash (assumed clock: unknown)
Erased/Wrote page  0-1 with 7160 bytes in 2491msec
Flash write Done


When I push the icon "Program Flash" option "Conection options -> Use JTAG interface" is inactive.

What could be the cause of working only in SWD ?

BTW. I program LPC4088, which is certainly JTAG.
0 项奖励
回复

1,686 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jan 17 01:07:07 MST 2014
SWD vs JTAG is selected in the IDE - it is not something you switch physically.

When starting a debug session, The IDE will automatically select the most appropriate connection type for your target (some LPC parts are StD only, some are both SWD and JTAG, and some are JTAG only).

See http://www.lpcware.com/content/faq/lpcxpresso/launch-configuration-menu

On the Debugger tab (at the bottom of the dialog - you will need to scroll) you will see a drop-down selection box. Select the JTAG option from the drop-down.
0 项奖励
回复