LPC-Link not working on Mac

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link not working on Mac

1,098 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by remcopoelstra on Fri May 30 02:03:45 MST 2014
Hi,

About half a year ago I bought a LPCXpresso LPC812 board. It worked nicely then.
In the mean time I've build my own board based on a LPC812 and wanted to use the LPC-Link as a debug probe.
I've disconnected the target board from the probe and connected the probe to my Mac. I've also downloaded LPCXpresso 7.2.0.
When I click the "boot" button, I get a dialog "Initializing LPC-Link....", which after 10 seconds gives the error that there was a timeout connecting to the LPC-Link. It does not matter whether my custom target board is connected to the LPC-Link or not.
The LPC-link does show up in the USB devices list (as a Philips Consumer Lifestyle product).

How can I get the LPC-Link to work?

Thanks in advance.

Kind regards,

Remco Poelstra
0 Kudos
Reply
2 Replies

1,041 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by remcopoelstra on Fri May 30 05:25:32 MST 2014
Thank you very much. Switching to the neighbouring USB port did indeed make the LPC-Link work.

Regards,

Remco Poelstra
0 Kudos
Reply

1,041 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 30 02:53:00 MST 2014
Please take a look at this old Code Red FAQ entry (which is still applicable):
http://www.support.code-red-tech.com/CodeRedWiki/LPCLinkMacOS

We will make this available in the LPCWare FAQs.
0 Kudos
Reply