LPC-Link not working but J-Link does

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC-Link not working but J-Link does

642件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nebarto on Tue Nov 06 20:13:58 MST 2012
I am debugging a LPC11xx part, with the J-Link on a custom board, this works totally fine. When I try to debug it with the LPC-Link, it gives me this error:


Quote:
Ni: LPCXpresso Debug Driver v4.0 (Sep 19 2012 09:03:23)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso43/lpcxpresso/bin/LPC11A02UK.xml

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso43/lpcxpresso/bin/nxp_directory.xml

Nc: Found generic directory XML file in C:/nxp/LPCXpresso43/lpcxpresso/bin/crt_directory.xml

Ed:02: Failed on connect: Ee(07). Bad ACK returned from status - wire error.
Et: Emu(0): Connected. Was: None. DpID:  3200066. Info: HID32HS12
Error 0: (null)
Last sticky: 0. AIndex: 0
No MemAp selected
No Speed test
SWD Frequency: 50 KHz. RTCK: False. Vector catch: False.
Packet delay: 0  Poll delay: 0.



What could be causing this?
0 件の賞賛
返信
1 返信

629件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Wed Nov 07 00:38:23 MST 2012
Search this forum with the sticky thread at the top of this forum.
This topic has been discussed previously.
0 件の賞賛
返信