LPC-Link doesn't work on windows8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link doesn't work on windows8.1

2,297 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ruru on Mon Oct 28 07:40:11 MST 2013
Hello,

I'am using lpcxpresso LPC1769 and lpcxpresso v6.1.0.
I can program flash by using program flash tool, but  cannot debug. When i tried to start debug, these message were shown:

751,066 12-target-select extended-remote | crt_emu_cm3_nxp -msg-port=57440 -g -mi -2 -pLPC1769 -vend\
or=NXP -e0 -wire=hid -flash-driver=LPC175x_6x_512.cfx
873,220 12^error,msg="Remote communication error.  Target disconnected.: No error."

My board is not broken because i can debug the same program by using another PC(windows vista).
I've already tried
- re-install DFU driver
- disable firewall
- exchange USB cable and port

thank you.
0 Kudos
Reply
9 Replies

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moisescatala on Thu Nov 27 15:09:08 MST 2014

Quote:

ruru - it is possible to use LPC-Link in an alternative 'winusb' mode on Windows, rather than as a HID device.

To do this, go to

Window - Preferences - LPCXpresso - LPC-Link

and untick the option "Initialise LPC-Link as HID".

Then unplug your LPCXpresso board, plug it back in, and try debugging again. Can you now connect?




I have windows 8.1 and  option "Initialise LPC-Link as HID" whas selected.


I unselected it, unplugged and plugged it back and this solved my issue with debugging on  LPC-Link  with my LPC1769

Perfect!!!

LPCXpresso Support, thanks!!!
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Dec 15 14:55:23 MST 2013
Did you try the suggestion that lpcxpresso-support suggested?
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by primate on Sun Dec 15 13:21:14 MST 2013
Are there any updates on this matter since I have the same problem? Thank you.
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Nov 01 09:51:44 MST 2013
Tsuneo - thanks for the pointer - this is interesting. We'll look into this.

ruru -  it is possible to use LPC-Link in an alternative 'winusb' mode on Windows, rather than as a HID device.

To do this, go to

Window - Preferences - LPCXpresso - LPC-Link

and untick the option "Initialise LPC-Link as HID".

Then unplug your LPCXpresso board, plug it back in, and try debugging again. Can you now connect?

Regards,
LPCXpresso Support
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Tsuneo on Fri Nov 01 09:13:37 MST 2013
LPC-Link seems to apply vendor-specific HID

Windows 8.1 has introduced strict power management to vendor-specific HID devices.
It drops such HID devices into Suspend immediately after enumeration.
Workarounds are known, described in the first post of this MS forum topic,

"USB vendor defined usage HID forced to suspend under Win 8.1 Preview."
http://social.msdn.microsoft.com/Forums/en-US/8f671193-52e4-467b-be45-4532a2ef1182/usb-vendor-define...

Tsuneo
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ruru on Tue Oct 29 06:01:54 MST 2013
Ni: LPCXpresso Debug Driver v6.0 (Oct 16 2013 02:04:27 - crt_emu_cm3_nxp build 1
212)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/LPC17
69.xml

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpres
so/bin/nxp_directory.xml

Nc: Found generic directory XML file in C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/b
in/crt_directory.xml

AP Ack: 04
Nc: Mem-AP ID: 0x24770011  ROM Addr: 0xE00FF003
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: HID64HS12
Nc: SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: Loaded LPC175x_6x_512.cfx: LPC175x_6x (512K) Apr 22 2013 12:14:31  On-chip F
lash Memory

Nc: NXP: LPC1769  Part ID: 0x00000000
Chip=LPC1769, from NXP (formerly Philips), in family LPC17xx, version=unknown
Chip Description: NXP LPC1769
ClockFreq=100.0MHz (Accurate). Clock can be changed after reset.
System reset doesn't cause power cycle. Last reset cause(s): PowerOn
Does have Flash and is programmable. 128M pop Mask: 0001
Mem MFlash512 of type Flash from 0000 for 524288 bytes. RO
Mem RamLoc32 of type RAM from 10000000 for 32768 bytes.
Mem RamAHB32 of type RAM from 2007c000 for 32768 bytes.
PrgFlash from 0000 to 80000 (524288 bytes). 2 Variable sized page rules (16 4K,1
4 32K)
  'Word' width: 4. Cannot read after programming starts
Peripheral TIMER3 at 0x40094000, size=64. Is part of Chip
  Timer
  Enabled by SYSCTL.PCONP.PCTIM3&0x1
Peripheral TIMER2 at 0x40090000, size=64. Is part of Chip
  Timer
  Enabled by SYSCTL.PCONP.PCTIM2&0x1
Peripheral TIMER1 at 0x40008000, size=64. Is part of Chip
  Timer
  Enabled by SYSCTL.PCONP.PCTIM1&0x1
Peripheral TIMER0 at 0x40004000, size=64. Is part of Chip
  Timer
  Enabled by SYSCTL.PCONP.PCTIM0&0x1
Peripheral SPI at 0x40020000, size=31. Is part of Chip
  SPI Interface
  Enabled by SYSCTL.PCONP.PCSPI&0x1
Peripheral MPU at 0xE000ED90, size=188. Is part of Chip
  MPU
Peripheral GPIO4 at 0x2009C080, size=32. Is part of Chip
  General Purpose IO
  Enabled by SYSCTL.PCONP.PCGPIO&0x1
Peripheral GPIO3 at 0x2009C060, size=32. Is part of Chip
  General Purpose IO
  Enabled by SYSCTL.PCONP.PCGPIO&0x1
Peripheral GPIO2 at 0x2009C040, size=32. Is part of Chip
  General Purpose IO
  Enabled by SYSCTL.PCONP.PCGPIO&0x1
Peripheral GPIO1 at 0x2009C020, size=32. Is part of Chip
  General Purpose IO
  Enabled by SYSCTL.PCONP.PCGPIO&0x1
Peripheral GPIO0 at 0x2009C000, size=32. Is part of Chip
  General Purpose IO
  Enabled by SYSCTL.PCONP.PCGPIO&0x1
Peripheral I2S at 0x400A8000, size=53. Is part of Chip
  I2S
  Enabled by SYSCTL.PCONP&0x08000000
Peripheral PCB at 0x4002C000, size=124. Is part of Chip
  Pin Control Block
Peripheral SYSCTL at 0x400FC000, size=460. Is part of Chip
  System control block
Peripheral DAC at 0x4008C000, size=11. Is part of Chip
  DAC
  Enabled by PCB.PINSEL1.P0_26&0x2=2
Peripheral SSP1 at 0x40030000, size=40. Is part of Chip
  SSP Interface
  Enabled by SYSCTL.PCONP.PCSSP1&0x1
Peripheral SSP0 at 0x40088000, size=40. Is part of Chip
  SSP Interface
  Enabled by SYSCTL.PCONP.PCSSP0&0x1
Peripheral CANAFR at 0x4003C000, size=32. Is part of Chip
  CAN Acceptance Filter Registers
  Enabled by SYSCTL.PCONP.PCCAN1&0x1|SYSCTL.PCONP.PCCAN2&0x1
Peripheral CANCEN at 0x40040000, size=12. Is part of Chip
  Central CAN Registers
  Enabled by SYSCTL.PCONP.PCCAN1&0x1|SYSCTL.PCONP.PCCAN2&0x1
Peripheral CANCON2 at 0x40048000, size=96. Is part of Chip
  CAN Controller Registers
  Enabled by SYSCTL.PCONP.PCCAN2&0x1
Peripheral CANCON1 at 0x40044000, size=96. Is part of Chip
  CAN Controller Registers
  Enabled by SYSCTL.PCONP.PCCAN1&0x1
Peripheral CANWAKESLEEP at 0x400FC110, size=8. Is part of Chip
  CAN Wake and Sleep Registers
Peripheral ADC at 0x40034000, size=56. Is part of Chip
  Analog to Digital Converter
  Enabled by SYSCTL.PCONP.PCAD&0x1
Peripheral USBDEV at 0x5000C200, size=4092. Is part of Chip
  USB Device Controller  (You need to set PCONP.PCUSB and the USBCLKCTL bits to
access this)
  Enabled by USBCLKCTL.USBClkSt&0x12=0x12
Peripheral PWM at 0x40018000, size=116. Is part of Chip
  PWM
  Enabled by SYSCTL.PCONP.PWM1&0x1
Peripheral I2C2 at 0x400A0000, size=64. Is part of Chip
  I2C Interface
  Enabled by SYSCTL.PCONP.PCI2C2&0x1
Peripheral I2C1 at 0x4005C000, size=64. Is part of Chip
  I2C Interface
  Enabled by SYSCTL.PCONP.PCI2C1&0x1
Peripheral I2C0 at 0x4001C000, size=64. Is part of Chip
  I2C Interface
  Enabled by SYSCTL.PCONP.PCI2C0&0x1
Peripheral DMA at 0x50004000, size=500. Is part of Chip
  DMA Controller
  Enabled by SYSCTL.PCONP.PCGPDMA&0x1
Peripheral ENET at 0x50000000, size=4088. Is part of Chip
  Ethernet MAC
  Enabled by SYSCTL.PCONP.PCENET&0x1
Peripheral DCR at 0xE000EDF0, size=16. Is part of Chip
  M3 Debug Core Registers
Peripheral QEI at 0x400BC000, size=4080. Is part of Chip
  Quadrature Encoder Interface
  Enabled by SYSCTL.PCONP.PCQEI&0x1
Peripheral USBHOST at 0x5000C000, size=4092. Is part of Chip
  USB Host Controller  (You need to set PCONP.PCUSB and the USBCLKCTL bits to ac
cess this)
  Enabled by USBCLKCTL.USBClkSt&0x11=0x11
Peripheral USBOTG at 0x5000C000, size=4092. Is part of Chip
  USB OTG Controller (You need to set PCONP.PCUSB and the USBCLKCTL bits to acce
ss this)
  Enabled by USBCLKCTL.USBClkSt&0x1c=0x1c
Peripheral NVIC at 0xE000E000, size=3844. Is part of Chip
  NVIC M3 Control/Status Regsiters
Peripheral RTC at 0x40024000, size=134. Is part of Chip
  Real time clock
  Enabled by SYSCTL.PCONP.PCRTC&0x1
Peripheral WDT at 0x40000000, size=20. Is part of Chip
  Watchdog Timer
Peripheral UART1 at 0x40010000, size=85. Is part of Chip
  UART
  Enabled by SYSCTL.PCONP.PCUART1&0x1
Peripheral UART3 at 0x4009C000, size=88. Is part of Chip
  UART
  Enabled by SYSCTL.PCONP.PCUART3&0x1
Peripheral UART2 at 0x40098000, size=88. Is part of Chip
  UART
  Enabled by SYSCTL.PCONP.PCUART2&0x1
Peripheral UART0 at 0x4000C000, size=88. Is part of Chip
  UART
  Enabled by SYSCTL.PCONP.PCUART0&0x1
Peripheral USBCLKCTL at 0x5000CFF4, size=8. Is part of Chip
  USB Clock Control (you need to have set PCONP.PCUSB to write these registers)
Peripheral USBINTSTAT at 0x400FC1C0, size=4. Is part of Chip
  USB Interrupt Status  (You need to set PCONP.PCUSB and the USBCLKCTL bits to a
ccess this)
  Enabled by USBCLKCTL.USBClkCtrl&0x12
Peripheral FLASHACCEL at 0x400FC000, size=4. Is part of Chip
  Flash Accelerator Configuration register
Peripheral GPIOINTMAP at 0x40028080, size=56. Is part of Chip
  GPIO Interrupt Register Map
Peripheral MCPWM at 0x400B8000, size=120. Is part of Chip
  Motor Control Pulse Width Modulator
  Enabled by SYSCTL.PCONP.PCMCPWM&0x1
Peripheral RIT at 0x400B0000, size=16. Is part of Chip
  Repetitive Interrupt Timer
  Enabled by SYSCTL.PCONP.PCRIT&0x1
Peripheral FMC at 0x40084000, size=4076. Is part of Chip
  Flash Module
<link href="file:///C:/nxp/LPCXpresso_6.1.0_164/lpcxpresso/bin/nxp_lpcxxxx_peri
pheral.xme" type="simple" show="embed" />
CPUID=0x410FC230, Little-Endian. Name=CM3, Chip=LPC1769,
CpuNum=3, Rev=0.0, MaxInts=64, SysTickCal=F423F
State is: Stopped (Was Running)  (stop cause: Halt)
Emulator support: 'Code Red HID emulator support for Cortex-M', version: 2.0
Connected to emu0: 'HID64HS12'
Connection state: ConnAndReset. DP ID=2BA01477. Sticky=10
Speed=1. Frequency=3000KHz. Packet delay=0, Poll delay=0. Info from speed test.
Retries=0. Since last Info request: 0
AP is_sel=SEL. AP rel idx=0 for ID=24770011
ROM table @E00FF003. Debug is OK. Bank=0, CtrlBase=23000000
0 devices:
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Oct 29 02:16:31 MST 2013
Please post the output from running the diagnostics described in...

http://support.code-red-tech.com/CodeRedWiki/LPCLinkDiagnostics

For Windows 8, please use the options in the FAQ as for Windows 7.

Regards,
LPCXpresso Support
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ruru on Tue Oct 29 01:41:11 MST 2013
I selected Debug messages from pull-down list, but it is blank.

when i try to debug, this dialog appear

Error in final launch sequence
  Failed to execute MI command:
-target-select extended-remote | crt_emu_cm3_nxp -msg-port=60226 -g -mi -2 -pLPC1769 -vendor=NXP -e0 -wire=hid -flash-driver=LPC175x_6x_512.cfx
Error message from debugger back end:
Remote communication error.  Target disconnected.: No error.
  Remote communication error.  Target disconnected.: No error.
0 Kudos
Reply

2,238 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Oct 28 21:31:11 MST 2013
Please post your debug log:
http://www.lpcware.com/content/faq/lpcxpresso/debug-log
0 Kudos
Reply