LPC-Link 2 CMSIS-DAP Firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-Link 2 CMSIS-DAP Firmware

949 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sgstreet on Sun Apr 13 12:11:41 MST 2014
I have a LPC Link 2 and I'm trying to flash the CMSIS-DAP firmware onto the board.  I used LPC_Link2_Config_tool_v1_11_1 to successfully flash the image (i.e. LPC-Link 2 Configuration Tool reported "Image verified by read back successfully"). When I install JP1 and attach the USB cable LED1 does not stay on and the LPC Link 2 does not enumerate on the USB bus.  LED1 flickers on briefly and then turns off.

Has anyone sucessfully flash the CMSIS-DAP firmware from the v1.11.1?  Any ideas on how to debug this problem?
0 Kudos
Reply
1 Reply

842 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Sun Apr 13 21:04:44 MST 2014
Hi sgstreet,
Yes I checked it after your post. Yes LED turns off,however it works without any problem. I tested it on MCB1500 board. I was able to flash and debug.
0 Kudos
Reply