LPC-LINK USB Driver Install Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC-LINK USB Driver Install Problem

9,672 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Sat Apr 10 09:19:34 MST 2010
Hello,

I just got my LPC-Xpress board
and when I try to install USB driver for LPC-Link
Windows XP does not recognized the tool.

I am using Windows XP Service Pack 3.

Any Ideas?
0 Kudos
Reply
19 Replies

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Apr 22 08:03:59 MST 2012
Whenever you plugin LPC-Link, you will never see LPC-Link displayed. This is because it needs booting- it powers on as a DFU device.

Booting LPC-Link is done automatically when you start a debug session, or you can boot it manually by following the instructions here.
http://support.code-red-tech.com/CodeRedWiki/CommandLineFlashProgramming

BTW: Unless you are doing something unusual, you should never need to boot it manually.
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Apr 22 07:40:32 MST 2012

Quote: swarandeep
I can't see any LPC- Link device?



If there's no 'Unknown device' left your Vista didn't install the driver :eek:

Either you've forgotten that or something has prevented installation (antivirus / firewall) :rolleyes:
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by swarandeep on Sun Apr 22 07:09:45 MST 2012

Quote: Moises
Yes,
I did everything you suggested.
I backup on the driver changes.

I plug in my LPC-Link board Windows XP did not see it
I went to Device Manager and found a ? mark on USB device, which was
the LPC-Link.  Then I told Windows to Update Driver, browsed to:
C:\nxp\lpcxpresso_3.2\Drivers\LPC-Link   which is were I install Code-Red

Windows then did its installation and saw LPC-Link then device manager
showed it under Universal Serial Bus Controllers.

Then I run Code-Red imported the Blink project compile, then told to debug
and I got message window that saying that could not debug because a LPC-Link
could not be found.




I'm having the same problem. When I plug in the LPCxpresso board in the USB port, the LED2 is flashing. I'm running Windows Vista and under device manager I can't see any LPC- Link device? Can anyone please help...
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Spencer on Thu Jun 16 22:51:29 MST 2011
Dear sirs:

There are some errors as attached file.

How to deal with it?
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Apr 14 11:40:28 MST 2010
Did you read this - especially the short article on using LPCXpresso with a VM?
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/49
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dphillps on Wed Apr 14 10:50:55 MST 2010
Environment:
I am using Ubuntu,VirtualBox (host), Windows XP Pro service pack 3 (Client). 
I have the LPC1114 board connected via USB and the red LED 2 is blinking.

Windows Device Manager shows: USB Device with DFU Capabilities.
Properties:
General:
  This device is working properly.
Driver:
  Driver Date: 2/10/2003
  Driver Version 3.10.0.0
Details:
Device Instance, USB\VID_0471&PID_DF55&C1E6CCE&0&1

Problem: When I try to debug blinky, LPC-Link v1.1 indicates a timeout problem.  "Timeout waiting for LPC-link v1.1 to initialize.  If this is the firt use after installation, your drivers may not have finished loading  Continue waiting. [yes/no]

Solution: Restart windows, now windows device manager shows: LPC-link debug probe v1.1
Clunky, but workable.
0 Kudos
Reply

8,336 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Tue Apr 13 12:57:18 MST 2010
Hi,

Great!

Thanks.:p
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Apr 13 06:32:37 MST 2010
Thanks for tracking this down.

FYI, We have made a small improvement to the DFU driver in the v3.3 release (which should be released later today, or tomorrow) to try to force Windows to re-enumerate the USB devices after the LPC-Link has been booted. It as an improvement, but it doesn't seem to work on all motherboards :-)
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Tue Apr 13 06:05:57 MST 2010
Hello CodeRed Support team,

I am terribly sorry for causing such confusion,
but I finally figure out what my problem was.

It turna out that my asus motherboard with AMD processor
does not enumerate USB devices very well for some unknown reason.
I am still looking into that. Any way.

After looking at Microsoft suggestions regarding USB drivers and without any luck.
I finally decided to manually search the registry and manually delete any entries
that the previous installation had made.  Once I got rid off them, I disconnected the LPC-Link board and restarted my system.

After it had booted, I plugged in the LPC-Link Board again, Windows did not recognized it again, so I manually installed the driver using Device Manager pointing windows to the c:\nxp\lpcxpresso_3.2\Drivers\DFU\MassDfu.inf file
then windows installed this driver.

After all this, I run Code Red IDE, compile blink project, then run a debug session
in which this time The LPC-Link Flash Screen appeared.  I was not done yet,
I had to once again go to Device Manager and tell Windows to install the LPC-Link Probe driver from this inf file c:\nxp\lpcxpresso_3.2\Drivers\LPC-Link.

After all this, Code Red finally saw the Debugger.

What a mess.

Any how.

Thanks for all the suggestions even though none worked in my case.  You know some times you have to hack windows in order to do things right.
:cool:
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Apr 13 00:02:36 MST 2010
Can you head over to the <install>/bin/Scripts directory and (from the command line) run 'bootLPCXpresso winusb'

This function is performed by the IDE when you start a debug session, but it might give some clues as to what is wrong with your setup.

When you first connect the board, Device Manager will report a "USB Device with DFU Capabilities" (this has a VID/PID of 0471/df55). After you have run the script (on XP) you will see "LPC-Link Debug Probe" (this has a VID/PID of 1fc9/9).

If this doesn't work, head back to the Scripts directory and run 'bootLPCXpresso' (without parameters). This will boot LPC-Link as a HID device (with a VID/PID of 1fc9/7).

Regardless of the way the LPC-Link is booted, the IDE will find it.
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Mon Apr 12 21:36:48 MST 2010
Hello,

I checked out the User Manual of the LPC315X
and found out that the on board DC/DC converters may or may not
be needed.

So  the board is using LDO regulators from USB BUS Power.
Therefore, there is something else wrong.
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Mon Apr 12 21:28:25 MST 2010
Hello,

After hours of search and trying out what can be happening,
I started troubleshooting my LPC-Link board and found
that the L1 and L2 are missing on my hardware.

PSU_LX1 and PSU_LX2 have no inductors for the DC/DC
on chip converters therefore PSU_Vout1 and PSU_Vout2 are wrong.

I am already falling behind contest.
Can you guys tell me if I can send back and you guys send another one?
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Mon Apr 12 13:21:58 MST 2010
Yes,
I did everything you suggested.
I backup on the driver changes.

I plug in my LPC-Link board Windows XP did not see it
I went to Device Manager and found a ? mark on USB device, which was
the LPC-Link.  Then I told Windows to Update Driver, browsed to:
C:\nxp\lpcxpresso_3.2\Drivers\LPC-Link   which is were I install Code-Red

Windows then did its installation and saw LPC-Link then device manager
showed it under Universal Serial Bus Controllers.

Then I run Code-Red imported the Blink project compile, then told to debug
and I got message window that saying that could not debug because a LPC-Link
could not be found.
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Apr 12 07:25:34 MST 2010
Please tell us exactly what you mean by "The driver installs but Code Red does not see it.":
- which driver installs?
- what error are you getting from the IDE?
- do you see the "Initialising LPC-Link" splash screen?
- did you backout the change you made to the driver?
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Mon Apr 12 05:54:05 MST 2010
Hello Xpresso Team,

I try all that you suggested and still
having problems with Code Red not seeing the LPC-Link board.

The driver installs but Code Red does not see it.

I don't know what else to try.

Any Ideas?
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun Apr 11 02:06:23 MST 2010
Hi,

Changing the VID/PID in the driver is the WRONG THING TO DO, and you will ensure now that it will never work Please change them back (a re-install will not help as Windows will see that the latest driver is installed and will not replace it). The VID/PID that you report, and the drivers, as supplied, are all correct.

For information on what is happening and why there are *two* drivers, please read:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/47
(login required)

You might also want to read:
http://lpcxpresso.code-red-tech.com/LPCXpresso/node/45

If doing this still doesn't help, try changing the following preference:
Windows->Preferences
+ LPCXpress
+ Debug
and check "Initialise LPC-Link and HID"
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Sat Apr 10 20:34:01 MST 2010
Hello,

After changing the VID and PID
and Windows XP finally allowing me to install driver.

But Now there is another problem,
Code Red IDE does not see the LPC-Link Debugger.

Windows install the Driver with modified VID and PID and shows
the LPC-Link under Universal Serial Bus Controllers under the name:
LPC-Link Debug Probe v1.1

Any Ideas?
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by moises on Sat Apr 10 10:05:03 MST 2010
Yes I did.

I figured out what the problem was.

For some unknown reason my Win XP
enumerated the LPC-Link with the following:
VID 0471 and PID DF55

But the LPC-Link Driver that came with Code Red
has VID 1FC9 PID 0009

Windows could not recognized the hardware,
So what I did was to manually change the Drivers VID and PID.

That allow windows to see the hardware and install the driver.

Thanks.
0 Kudos
Reply

8,337 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Sat Apr 10 09:57:47 MST 2010
Did you install LPCXpresso IDE? It includes the drivers.
0 Kudos
Reply