LPC Expresso Tool chain Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC Expresso Tool chain Error

1,016件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomathivanan on Fri Jul 15 21:56:22 MST 2011
[B]I am getting the following error when build my project:[/B]
I am not able build the project.
**** Clean-only build of configuration Debug for project CORTEXM0PRINTERV1.0 ****

make clean
      0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0x0, BaseAddress 0x7A0000, RegionSize 0x30000, State 0x10000
C:\nxp\LPCXpresso_4.0.5_123\lpcxpresso\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0
0 件の賞賛
返信
2 返答(返信)

986件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tomathivanan on Sat Jul 16 01:17:58 MST 2011
After replacement of the dll, the compilation time is more. which i compared with my old PC dual core 1.6GHz & 1GB DDR2 RAM and the current system i7 2.9GHz 4GB DDR3. in both the cases other then espresso no active program & same code. What this dll does. .? how to improve the compilation speed.
0 件の賞賛
返信

986件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sat Jul 16 00:40:09 MST 2011
Did you look in the FAQ?
http://support.code-red-tech.com/CodeRedWiki/VirtualAllocPointerNull
0 件の賞賛
返信