LPC 1769, cant debug!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC 1769, cant debug!

1,829件の閲覧回数
basilejuanignac
Contributor I

Hey everyone, here's my problem. I cant debug the LPC 1769 with my projects. Don't know why, but what i know is that i have no errors in my project because when i try to debug an ancient one it does the same thing. What thing?. Well the lpc link does blink when im trying to debug, but when it's all done the lpc turns on the internal led with half power.

What can i do?

Thanks,

Juafra

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,639件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

What target board are you using? Is it an off-the-shelf board or one of your own design?

What debug probe are you using? Is it the original LPC-Link, an LPC-Link2, or something else?

What version of LPCXpresso IDE are you using?

Have you tried booting your board into ISP mode ?

If you are still having problems, can you post your debug log?

Regards,

LPCXpresso Support

0 件の賞賛
返信

1,639件の閲覧回数
converse
Senior Contributor V

From your description, the application is working, but the you have no delay between the on and off states of the LED. If you flash the LED very quickly, it will appear to be on with 50% brightness.

0 件の賞賛
返信