LPC 1769 UARTrecieve

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1769 UARTrecieve

1,359 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rhlmhrtr on Sun May 11 23:27:43 MST 2014
Hi I am trying to read data from LPC 1769 uart.
I went through the sameple code and I found that i can use it only to send data and not to recieve it.
I am very new to LPC 1769 programming and it would be really great if someone can point me in the right direction.


/***********************************************************************
 * $Id::                                                               $
 *
 * Project:uart: Simple UART echo for LPCXpresso 1700
 * File:uart.c
 * Description:
 * LPCXpresso Baseboard uses pins mapped to UART3 for
 * its USB-to-UART bridge. This application simply echos
 * all characters received.
 *
 ***********************************************************************
 * Software that is described herein is for illustrative purposes only
 * which provides customers with programming information regarding the
 * products. This software is supplied "AS IS" without any warranties.
 * NXP Semiconductors assumes no responsibility or liability for the
 * use of the software, conveys no license or title under any patent,
 * copyright, or mask work right to the product. NXP Semiconductors
 * reserves the right to make changes in the software without
 * notification. NXP Semiconductors also make no representation or
 * warranty that such application will be suitable for the specified
 * use without further testing or modification.
 **********************************************************************/

/*****************************************************************************
 *   History
 *   2010.07.01  ver 1.01    Added support for UART3, tested on LPCXpresso 1700
 *   2009.05.27  ver 1.00    Prelimnary version, first Release
 *
******************************************************************************/
#include "LPC17xx.h"
#include "type.h"
#include "uart.h"

volatile uint32_t UART0Status, UART1Status, UART3Status;
volatile uint8_t UART0TxEmpty = 1, UART1TxEmpty = 1, UART3TxEmpty=1;
volatile uint8_t UART0Buffer[BUFSIZE], UART1Buffer[BUFSIZE], UART3Buffer[BUFSIZE];
volatile uint32_t UART0Count = 0, UART1Count = 0, UART3Count = 0;

/*****************************************************************************
** Function name:UART0_IRQHandler
**
** Descriptions:UART0 interrupt handler
**
** parameters:None
** Returned value:None
** 
*****************************************************************************/
void UART0_IRQHandler (void) 
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_UART0->IIR;
    
  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if ( IIRValue == IIR_RLS )/* Receive Line Status */
  {
LSRValue = LPC_UART0->LSR;
/* Receive Line Status */
if ( LSRValue & (LSR_OE|LSR_PE|LSR_FE|LSR_RXFE|LSR_BI) )
{
  /* There are errors or break interrupt */
  /* Read LSR will clear the interrupt */
  UART0Status = LSRValue;
  Dummy = LPC_UART0->RBR;/* Dummy read on RX to clear 
interrupt, then bail out */
  return;
}
if ( LSRValue & LSR_RDR )/* Receive Data Ready */
{
  /* If no error on RLS, normal ready, save into the data buffer. */
  /* Note: read RBR will clear the interrupt */
  UART0Buffer[UART0Count] = LPC_UART0->RBR;
  UART0Count++;
  if ( UART0Count == BUFSIZE )
  {
UART0Count = 0;/* buffer overflow */
  }
}
  }
  else if ( IIRValue == IIR_RDA )/* Receive Data Available */
  {
/* Receive Data Available */
UART0Buffer[UART0Count] = LPC_UART0->RBR;
UART0Count++;
if ( UART0Count == BUFSIZE )
{
  UART0Count = 0;/* buffer overflow */
}
  }
  else if ( IIRValue == IIR_CTI )/* Character timeout indicator */
  {
/* Character Time-out indicator */
UART0Status |= 0x100;/* Bit 9 as the CTI error */
  }
  else if ( IIRValue == IIR_THRE )/* THRE, transmit holding register empty */
  {
/* THRE interrupt */
LSRValue = LPC_UART0->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
if ( LSRValue & LSR_THRE )
{
  UART0TxEmpty = 1;
}
else
{
  UART0TxEmpty = 0;
}
  }
}

/*****************************************************************************
** Function name:UART1_IRQHandler
**
** Descriptions:UART1 interrupt handler
**
** parameters:None
** Returned value:None
** 
*****************************************************************************/
void UART1_IRQHandler (void) 
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_UART1->IIR;
    
  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if ( IIRValue == IIR_RLS )/* Receive Line Status */
  {
LSRValue = LPC_UART1->LSR;
/* Receive Line Status */
if ( LSRValue & (LSR_OE|LSR_PE|LSR_FE|LSR_RXFE|LSR_BI) )
{
  /* There are errors or break interrupt */
  /* Read LSR will clear the interrupt */
  UART1Status = LSRValue;
  Dummy = LPC_UART1->RBR;/* Dummy read on RX to clear 
interrupt, then bail out */
  return;
}
if ( LSRValue & LSR_RDR )/* Receive Data Ready */
{
  /* If no error on RLS, normal ready, save into the data buffer. */
  /* Note: read RBR will clear the interrupt */
  UART1Buffer[UART1Count] = LPC_UART1->RBR;
  UART1Count++;
  if ( UART1Count == BUFSIZE )
  {
UART1Count = 0;/* buffer overflow */
  }
}
  }
  else if ( IIRValue == IIR_RDA )/* Receive Data Available */
  {
/* Receive Data Available */
UART1Buffer[UART1Count] = LPC_UART1->RBR;
UART1Count++;
if ( UART1Count == BUFSIZE )
{
  UART1Count = 0;/* buffer overflow */
}
  }
  else if ( IIRValue == IIR_CTI )/* Character timeout indicator */
  {
/* Character Time-out indicator */
UART1Status |= 0x100;/* Bit 9 as the CTI error */
  }
  else if ( IIRValue == IIR_THRE )/* THRE, transmit holding register empty */
  {
/* THRE interrupt */
LSRValue = LPC_UART1->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
if ( LSRValue & LSR_THRE )
{
  UART1TxEmpty = 1;
}
else
{
  UART1TxEmpty = 0;
}
  }

}
/*****************************************************************************
** Function name:UART0_IRQHandler
**
** Descriptions:UART0 interrupt handler
**
** parameters:None
** Returned value:None
**
*****************************************************************************/
void UART3_IRQHandler (void)
{
  uint8_t IIRValue, LSRValue;
  uint8_t Dummy = Dummy;

  IIRValue = LPC_UART3->IIR;

  IIRValue >>= 1;/* skip pending bit in IIR */
  IIRValue &= 0x07;/* check bit 1~3, interrupt identification */
  if ( IIRValue == IIR_RLS )/* Receive Line Status */
  {
LSRValue = LPC_UART3->LSR;
/* Receive Line Status */
if ( LSRValue & (LSR_OE|LSR_PE|LSR_FE|LSR_RXFE|LSR_BI) )
{
  /* There are errors or break interrupt */
  /* Read LSR will clear the interrupt */
  UART3Status = LSRValue;
  Dummy = LPC_UART3->RBR;/* Dummy read on RX to clear
interrupt, then bail out */
  return;
}
if ( LSRValue & LSR_RDR )/* Receive Data Ready */
{
  /* If no error on RLS, normal ready, save into the data buffer. */
  /* Note: read RBR will clear the interrupt */
  UART3Buffer[UART3Count] = LPC_UART3->RBR;
  UART3Count++;
  if ( UART3Count == BUFSIZE )
  {
UART3Count = 0;/* buffer overflow */
  }
}
  }
  else if ( IIRValue == IIR_RDA )/* Receive Data Available */
  {
/* Receive Data Available */
UART3Buffer[UART3Count] = LPC_UART3->RBR;
UART3Count++;
if ( UART3Count == BUFSIZE )
{
  UART3Count = 0;/* buffer overflow */
}
  }
  else if ( IIRValue == IIR_CTI )/* Character timeout indicator */
  {
/* Character Time-out indicator */
UART3Status |= 0x100;/* Bit 9 as the CTI error */
  }
  else if ( IIRValue == IIR_THRE )/* THRE, transmit holding register empty */
  {
/* THRE interrupt */
LSRValue = LPC_UART3->LSR;/* Check status in the LSR to see if
valid data in U0THR or not */
if ( LSRValue & LSR_THRE )
{
  UART3TxEmpty = 1;
}
else
{
  UART3TxEmpty = 0;
}
  }
}


/*****************************************************************************
** Function name:UARTInit
**
** Descriptions:Initialize UART port, setup pin select,
**clock, parity, stop bits, FIFO, etc.
**
** parameters:portNum(0 or 1) and UART baudrate
** Returned value:true or false, return false only if the 
**interrupt handler can't be installed to the 
**VIC table
** 
*****************************************************************************/
uint32_t UARTInit( uint32_t PortNum, uint32_t baudrate )
{
  uint32_t Fdiv;
  uint32_t pclkdiv, pclk;

  if ( PortNum == 0 )
  {
LPC_PINCON->PINSEL0 &= ~0x000000F0;
LPC_PINCON->PINSEL0 |= 0x00000050;  /* RxD0 is P0.3 and TxD0 is P0.2 */
/* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
/* Bit 6~7 is for UART0 */
pclkdiv = (LPC_SC->PCLKSEL0 >> 6) & 0x03;
switch ( pclkdiv )
{
  case 0x00:
  default:
pclk = SystemCoreClock/4;
break;
  case 0x01:
pclk = SystemCoreClock;
break; 
  case 0x02:
pclk = SystemCoreClock/2;
break; 
  case 0x03:
pclk = SystemCoreClock/8;
break;
}

    LPC_UART0->LCR = 0x83;/* 8 bits, no Parity, 1 Stop bit */
Fdiv = ( pclk / 16 ) / baudrate ;/*baud rate */
    LPC_UART0->DLM = Fdiv / 256;
    LPC_UART0->DLL = Fdiv % 256;
LPC_UART0->LCR = 0x03;/* DLAB = 0 */
    LPC_UART0->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

   NVIC_EnableIRQ(UART0_IRQn);

    LPC_UART0->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART0 interrupt */
    return (TRUE);
  }
  else if ( PortNum == 1 )
  {
LPC_PINCON->PINSEL4 &= ~0x0000000F;
LPC_PINCON->PINSEL4 |= 0x0000000A;/* Enable RxD1 P2.1, TxD1 P2.0 */

/* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
/* Bit 8,9 are for UART1 */
pclkdiv = (LPC_SC->PCLKSEL0 >> 8) & 0x03;
switch ( pclkdiv )
{
  case 0x00:
  default:
pclk = SystemCoreClock/4;
break;
  case 0x01:
pclk = SystemCoreClock;
break; 
  case 0x02:
pclk = SystemCoreClock/2;
break; 
  case 0x03:
pclk = SystemCoreClock/8;
break;
}

    LPC_UART1->LCR = 0x83;/* 8 bits, no Parity, 1 Stop bit */
Fdiv = ( pclk / 16 ) / baudrate ;/*baud rate */
    LPC_UART1->DLM = Fdiv / 256;
    LPC_UART1->DLL = Fdiv % 256;
LPC_UART1->LCR = 0x03;/* DLAB = 0 */
    LPC_UART1->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

   NVIC_EnableIRQ(UART1_IRQn);

    LPC_UART1->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART1 interrupt */
    return (TRUE);
  }
  else if ( PortNum == 3 )
  {
  LPC_PINCON->PINSEL0 &= ~0x0000000F;
  LPC_PINCON->PINSEL0 |=  0x0000000A;  /* RxD3 is P0.1 and TxD3 is P0.0 */
  LPC_SC->PCONP |= 1<<4 | 1<<25; //Enable PCUART1
  /* By default, the PCLKSELx value is zero, thus, the PCLK for
all the peripherals is 1/4 of the SystemFrequency. */
  /* Bit 6~7 is for UART3 */
  pclkdiv = (LPC_SC->PCLKSEL1 >> 18) & 0x03;
  switch ( pclkdiv )
  {
  case 0x00:
  default:
  pclk = SystemCoreClock/4;
  break;
  case 0x01:
  pclk = SystemCoreClock;
  break;
  case 0x02:
  pclk = SystemCoreClock/2;
  break;
  case 0x03:
  pclk = SystemCoreClock/8;
  break;
  }
  LPC_UART3->LCR = 0x83;/* 8 bits, no Parity, 1 Stop bit */
  Fdiv = ( pclk / 16 ) / baudrate ;/*baud rate */
  LPC_UART3->DLM = Fdiv / 256;
  LPC_UART3->DLL = Fdiv % 256;
  LPC_UART3->LCR = 0x03;/* DLAB = 0 */
  LPC_UART3->FCR = 0x07;/* Enable and reset TX and RX FIFO. */

  NVIC_EnableIRQ(UART3_IRQn);

  LPC_UART3->IER = IER_RBR | IER_THRE | IER_RLS;/* Enable UART3 interrupt */
  return (TRUE);
  }
  return( FALSE ); 
}

/*****************************************************************************
** Function name:UARTSend
**
** Descriptions:Send a block of data to the UART 0 port based
**on the data length
**
** parameters:portNum, buffer pointer, and data length
** Returned value:None
** 
*****************************************************************************/
void UARTSend( uint32_t portNum, uint8_t *BufferPtr, uint32_t Length )
{
  if ( portNum == 0 )
  {
    while ( Length != 0 )
    {
  /* THRE status, contain valid data */
  while ( !(UART0TxEmpty & 0x01) );
  LPC_UART0->THR = *BufferPtr;
  UART0TxEmpty = 0;/* not empty in the THR until it shifts out */
  BufferPtr++;
  Length--;
}
  }
  else if (portNum == 1)
  {
while ( Length != 0 )
    {
  /* THRE status, contain valid data */
  while ( !(UART1TxEmpty & 0x01) );
  LPC_UART1->THR = *BufferPtr;
  UART1TxEmpty = 0;/* not empty in the THR until it shifts out */
  BufferPtr++;
  Length--;
    }
  }
  else if ( portNum == 3 )
  {
    while ( Length != 0 )
    {
  /* THRE status, contain valid data */
  while ( !(UART3TxEmpty & 0x01) );
  LPC_UART3->THR = *BufferPtr;
  UART3TxEmpty = 0;/* not empty in the THR until it shifts out */
  BufferPtr++;
  Length--;
}
  }
  return;
}

/******************************************************************************
**                            End Of File
******************************************************************************/
0 Kudos
Reply
2 Replies

1,096 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elektronist on Thu May 29 00:13:50 MST 2014
Hi rhlmhrtr, sorry for my late response.

This is a nice library and I use it too. It can be used for both receive and send. All receive task is done in the interrupt routine. To get received bytes just keep track of UARTxCount. Whenever you've got some bytes received, move them from UARTxBuffer to another buffer (you may use memcpy) and clear UARTxCount.

You can improve the code by using ring buffers.

0 Kudos
Reply

1,096 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rhlmhrtr on Sun May 11 23:32:08 MST 2014
I am using it to interface LPC 1769 with RN171, so I just need to read that data which is present on UART Rx
0 Kudos
Reply