LPC 1768 SPI Help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1768 SPI Help

1,440 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Shaoer on Mon Oct 29 13:03:10 MST 2012
I have been attempting to write a wireless communication code between LPC 1768 and wireless boards using SPI, there's really no example code to do it(The one on Code Red is for UART). Does anyone have anything I can use to learn/reference, considering this is my first time working with LPC?

Thanks a ton!!
0 Kudos
Reply
4 Replies

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Shaoer on Mon Oct 29 13:47:09 MST 2012
Thank you very much!! :)
0 Kudos
Reply

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Oct 29 13:29:21 MST 2012
I'm not familiar with your computer :), my LPCXpresso sample folder is in:

...\LPCXpresso_4.3.0_1023\lpcxpresso\Examples\NXP\LPC1000\LPC17xx

LPCXpresso should have installed this samples on your computer also ;)

See also: http://www.support.code-red-tech.com/CodeRedWiki/SuppliedExamples?highlight=%28examples%29
0 Kudos
Reply

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Shaoer on Mon Oct 29 13:21:56 MST 2012
Sorry about the ignorance, can you link me to this folder? I can't seem to find it :confused:
0 Kudos
Reply

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Oct 29 13:16:24 MST 2012

Quote: Shaoer
... no example code to do it...



:confused:

What's wrong with SPI / SSP samples in example folder?
0 Kudos
Reply