LPC 1768 Flash programming over ethernt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC 1768 Flash programming over ethernt

1,357 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tom_electronic on Wed Oct 12 02:52:41 MST 2011
hi


Is it possible to program lpc1768 over Ethernet ?

or  this MCU could be programmed over UART and  JTAG

your help is highly appreciated.
0 Kudos
Reply
4 Replies

1,149 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Mar 28 09:24:12 MST 2012
Just saw this thread and am about to try the same. Did you guys have any luck in doing this conversion to Ethernet? The advantage to Ethernet over USB is that we may be able to remotely flash a device already installed in the field without leaving our labs. Cheers!
0 Kudos
Reply

1,149 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tom_electronic on Wed Nov 09 05:03:00 MST 2011
hallo,

I'm trying to change it to be suitable for KEIL

any help is greatly appreciated
0 Kudos
Reply

1,149 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Thu Oct 13 00:59:32 MST 2011
The bootloader examples that Code Red provide for the board are a good starting point, and show the principles. The biggest problem you are going to have is that you need to have a minimal working TCP/IP stack (the bits required to transfer the data to the bootloader) inside the bootloader, as a complete TCP/IP stack may be too large to include in the bootloader.
0 Kudos
Reply

1,149 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by james on Thu Oct 13 00:36:28 MST 2011
Hi tom,

I am also currently working on a project which requires similar requirments.
Maybe you would like to check this:
http://knowledgebase.nxp.com/showthread.php?t=1540

I am also new to ARM programming, any additional help would certainly be appreciated.

My project requires the board to be connected to the internet to display data, change firmware via internet without any physical intervention.

Any tips on how to do this will be greatly appreciated.
I am currently using the RDB1768v2 demo board from red-code-tech
0 Kudos
Reply