JTAG with other LPC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG with other LPC

729件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgonzales52 on Wed Feb 10 11:32:15 MST 2010
I recently got a LPCXpresso board. I am also developing with an LPC2194 Quickstart board from Embedded Artists using Eclipse, gdb, and a wiggler paralel port jtag-interface. The cuestion is if I can use de USB JTAG of the LPCXpresso board with my old toolchain, or with other open source gdb based debugger ( insight for example)?.
Is there any document about the facts?
Thank you.
0 件の賞賛
返信
1 返信

715件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Feb 11 00:49:44 MST 2010
The LPCXpresso IDE supports only a small subset of the LPC2xxx family, and the LPC2194 is not amongst them.

The LPC-Link interface is currently only supported in LPCXpresso (and Red Suite).

There is an upgrade product from Code Red (Red Suite 3 - currently in beta) that supports the LPC2xxx family and LPC-Link.
0 件の賞賛
返信