JTAG in LPC1114

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG in LPC1114

1,497 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Mon Feb 15 04:27:16 MST 2010
UM, Table 90. IOCON_JTAG_TDI_PIO0_11 register (IOCON_JTAG_TDI_PIO0_11, address 0x4004 4074) bit description

2:0 FUNC Selects pin function. 000
000 Selects function TDI.

Does LPC1114 support JTAG?

Original Attachment has been moved to: 1100114_ssp.h.txt.zip

0 Kudos
Reply
4 Replies

1,409 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Wed Feb 17 14:51:29 MST 2010

Quote: rkiryanov
UM, Table 90. IOCON_JTAG_TDI_PIO0_11 register (IOCON_JTAG_TDI_PIO0_11, address 0x4004 4074) bit description

2:0 FUNC Selects pin function. 000
000 Selects function TDI.

Does LPC1114 support JTAG?



Func 000 on pin PIO0_11 is not supported because the LPC111x and LPC134x do not support JTAG. The Users Manual will be updated to reflect this.
0 Kudos
Reply

1,409 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Wed Feb 17 11:00:38 MST 2010
What option will be selected on IOCON_JTAG_TDI_PIO0_11.FUNC = 0?
0 Kudos
Reply

1,409 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rkiryanov on Mon Feb 15 05:58:38 MST 2010

Quote: CodeRedSupport
They are both SWD-only.



Hello,

what option will be selected on IOCON_JTAG_TDI_PIO0_11.FUNC = 0? When documentation update will be available?
Thanks.
0 Kudos
Reply

1,409 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Feb 15 05:15:40 MST 2010
Hi,

The LPC1100 and LPC1300 do not support JTAG for debug. They are both SWD-only.
0 Kudos
Reply