JTAG Configuration - No devices Found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JTAG Configuration - No devices Found

4,833 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Thu Jul 24 03:00:19 MST 2014
Hi!

I am using the LPC-Link2 board, that has a 10-pin JTAG, to program an evaluation board from waveshare, that has a 20-pin JTAG. I made a custom 10-pin to 20-pin adapter to be able to program the board.

I was able to program the board multiple times but sometimes I need to restart the process because the LPCXpresso cannot find the JTAG. At the moment, I cannot fix the problem and the IDE always give me the error "JTAG Configuration - No devices Found" (see figure)

I already tried to restart the IDE, power cycle both boards and reinstall the image on LPC-Link2 but without success.

I ask for help to discover if the problem if something related with software or hardware. I think that the custom adapter is the source of the problem but it worked quite well since I made it.

The log from Redlink Server was as shown below:

[Started server]
[Connected on port 3025]
redlink>
redlink>ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = 21BD, PID=0006
Path = \\?\hid#vid_21bd&pid_0006#7&4d934e&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
redlink>
redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = 21BD, PID=0006
Path = \\?\hid#vid_21bd&pid_0006#7&4d934e&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 64
Probe Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = REDLINK
redlink>
redlink>
redlink>
redlink>ProbeIsOpen 1
FALSE
redlink>ProbeOpenByIndex 1
Handle = 0x00000001 = 1
redlink>WireIsConnected 1
FALSE
redlink>WireJtagConnect 1
Error reading from server (redlinkserv.exe):
Read timed out
redlink>
Error reading from server (redlinkserv.exe):
Read timed out
[Closed]
[Started server]
[Connected on port 3025]
[Closed]
[Started server]
[Connected on port 3025]
redlink>
redlink>
redlink>ProbeStatus
redlink>exit
[Closed]
[Started server]
[Connected on port 3025]
redlink>
redlink>
redlink>ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = 21BD, PID=0006
Path = \\?\hid#vid_21bd&pid_0006#7&4d934e&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
redlink>
redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPCLINK2 Redlink
VID = 21BD, PID=0006
Path = \\?\hid#vid_21bd&pid_0006#7&4d934e&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 64
Probe Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = REDLINK
redlink>
redlink>
redlink>ProbeIsOpen 1
FALSE
redlink>ProbeOpenByIndex 1
Handle = 0x00000001 = 1
redlink>WireIsConnected 1
FALSE
redlink>WireJtagConnect 1
redlink>CoresConfigured 1
FALSE
redlink>CoreConfig 1
Number of CORES/TAPs = 0, Fully recognized: True
redlink>
redlink>CoreList 1
Error reading from server (redlinkserv.exe):
Read timed out
redlink>
Error reading from server (redlinkserv.exe):
Read timed out
[Closed]
[Started server]
[Connected on port 3025]
redlink>
redlink>
redlink>ProbeStatus
redlink>exit
[Closed]


Best Regards,
Hugo
0 Kudos
Reply
8 Replies

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lshl on Sun Mar 01 18:57:45 MST 2015
I am having the same problem (using LPC-Link2 for LPC1549).
The LPC-Link is just briked, it appears with VID/PID 0040/000C, when its supposed to be 1FC9/000C (that's what it was before it briked).
The red LED is not flashing.
Any suggestions?

Thanks
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Mon Jul 28 02:55:56 MST 2014
I tested my new adapter today and it works perfectly on my first try. Therefore, my problem was related with the JTAG connections, even though that my custom connection  had worked fine for several times.


Thanks for help,
Hugo
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Thu Jul 24 09:07:28 MST 2014
I will try other JTAG adapter and post here soon I have conclusions.

Thanks for help
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 24 09:01:14 MST 2014
We suspect a problem with your adapter. You might try using an SWD connection instead of JTAG as it uses the pins differently, but I am not that hopeful. See
http://www.lpcware.com/content/faq/lpcxpresso/connecting-jtag-target

Yes, the blinking LED is a new feature of the latest version of the firmware. It just a heartbeat and confirms the firmware is running.
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Thu Jul 24 08:32:33 MST 2014
Yes, I am using the latest version of LPCXpresso. I even tried with the previous versions (7.2 and 7.1.1)

I was able to program the board yesterday without problem and I did not do anything special in order to have problems.

I do not know if it matters but the LPC Link 2 have its LED blinking when I tried to program. I think that it did not have this behaviour in previous versions of LPCXpresso
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 24 08:17:53 MST 2014
Which version of LPCXpresso are you using? You should make sure you are using the latest - v7.3.0
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by HCTEK on Thu Jul 24 08:11:49 MST 2014
Hello,

my target is LPC4337JBD144.

Before your reply I did not tried that procedures. I tried both and nothing happens.

Regarding the first procedure, I connect the pin P2_7 to GND and assert the RST button that the waveshare evaluation board have. I tried to debug again and the same error appear. If I try again to debug, the redlink server must be restarted (see figure). I need to power cycle the LPC link 2 board in order to obtain the first error of "JTAG Configuration - no devices found".

The boot configuration is set to USART0 (all boot pins set to LOW).
0 Kudos
Reply

4,531 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 24 06:02:53 MST 2014
You haven't mentioned which target you are trying to program. Also, have you followed the instructions here?
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
0 Kudos
Reply