Invalid Project in Examples LPC1347 for LPCXpresso v5.2.6 [Build 2137] [2013-07-08] prevents IDE from listing archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Invalid Project in Examples LPC1347 for LPCXpresso v5.2.6 [Build 2137] [2013-07-08] prevents IDE from listing archive

578 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mathseng on Wed Jul 31 19:35:23 MST 2013
Issue Description:
Faulty project in file prevents IDE from listing archive contents.
Project LPCXpresso1347_systick contains corrupted files - all source files have (apparently) duplicated contents.

Archive containing faulty project:
C:\nxp\LPCXpresso_5.2.6_2137\lpcxpresso\Examples\NXP\LPC1000\LPC13xx_12bitADC\LPCXpresso1347.zip

Workaround #1:
Copy LPCXpresso1347.zip from the earlier LPCXpresso v5.2.4 Build 2122 release.
Workaround #2:
Make a backup copy of the .ZIP file, then Delete the directory LPCXpresso1347_systick from the .ZIP file - this does not recover the faulty project.

How to reproduce:
Quickstart > Import project(s) > Project archive (zip) Browse... > Next > [[[ no projects listed ]]

0 项奖励
回复
1 回复

567 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 01 01:07:04 MST 2013
That is very wierd. The reason you get no projects displayed is that the text duplication occurs in the project config files as well as the source files. I have no idea how this could have happened, as the files look fine inside our repository and the zips are created automatically by the build system. And none of this changed between 5.2.4 and 5.2.6 at all.

Anyway, I've attached a copy of this example ZIP (without the problem) to this thread in case anyone else encounters this.

Regards,
LPCXpresso Support
0 项奖励
回复