Interrupt levels in LPC11xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Interrupt levels in LPC11xx

1,428 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Wed Mar 14 08:48:59 MST 2012
Hi!
LPC11xx have 4 levels of interrupt.
How I can disable all interrupt of given level: for exsample disable/ enable interrupt of level 3 or 2. It is possible?
Thanks.
0 项奖励
回复
5 回复数

1,410 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Mar 15 07:43:21 MST 2012
FYI - You can do this on Cortex-M3 based parts like LPC13 and LPC17 using the NVIC's BASEPRI register, but not on Cortex-M0 based parts like LPC11 (which don't have this register implemented in their NVIC).

Regards,
CodeRedSupport
0 项奖励
回复

1,410 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Thu Mar 15 06:00:37 MST 2012

Quote: Zero
I know :rolleyes:
So the answer is still: there's no register or command to group enable/disable interrupts :(


I see.
Thanks.
0 项奖励
回复

1,410 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 14 10:37:50 MST 2012

Quote: ArtjomGromak
I meant such possibility...



I know :rolleyes:

If there would be such an option I wouldn't have suggested to read Priority Registers :)

So the answer is still: there's no register or command to group enable/disable interrupts :(
0 项奖励
回复

1,410 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Wed Mar 14 10:29:16 MST 2012
That is you suggest to write to 8 registers(IP0-IP7)?
It requires long time.

I meant such possibility: for example,  I will take the xmega processor (not ARM). Xmega have 3 interrupt levels. To disable level I must write to 1 register:
PMIC.CTRL&=(1<<LOLVLEN); // disable lowest priority level
PMIC.CTRL|=(1<<HILVLEN)|(1<<MEDLVLEN); // enable high and medium level

It is executed 4-5 commands.
Whether there is in Cortex-M0 something similar?
0 项奖励
回复

1,410 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Mar 14 09:10:40 MST 2012

Quote: ArtjomGromak
How I can disable all interrupt of given level: for exsample disable/ enable interrupt of level 3 or 2. It is possible?



Yes, write a function to read Interrupt Priority Registers and disable / enable all interrupts with appropriate value :rolleyes:
0 项奖励
回复