Internal Pull- ups in SPI protocol, LPC1317-64P

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Internal Pull- ups in SPI protocol, LPC1317-64P

841 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aamir ali on Mon Mar 04 00:07:47 MST 2013
1 .Since in MISO0 line is input pin, so is there need of using internal pull up of LPC1317, so avoid floating condition.

2. Or we can put pull up at both MISO & MOSI lines without problem.
If yes,MOSI is output pin so on having internal pull up enabled is right, or it will affect the circuit.

3. Or I should not use pull up with any of line.


I have interface SD card with SPI protocol
0 项奖励
回复
1 回复

821 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Mon Mar 04 04:47:50 MST 2013
Pull-ups aren't required for SPI.
0 项奖励
回复