Internal Pull- ups in SPI protocol, LPC1317-64P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal Pull- ups in SPI protocol, LPC1317-64P

823 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aamir ali on Mon Mar 04 00:07:47 MST 2013
1 .Since in MISO0 line is input pin, so is there need of using internal pull up of LPC1317, so avoid floating condition.

2. Or we can put pull up at both MISO & MOSI lines without problem.
If yes,MOSI is output pin so on having internal pull up enabled is right, or it will affect the circuit.

3. Or I should not use pull up with any of line.


I have interface SD card with SPI protocol
0 Kudos
Reply
1 Reply

803 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by leon_heller on Mon Mar 04 04:47:50 MST 2013
Pull-ups aren't required for SPI.
0 Kudos
Reply