Including the drivers folder in a new project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Including the drivers folder in a new project

951件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chris1seto on Wed Jul 13 21:54:20 MST 2011
In the LPC examples, I see several folders not added whe na new C project is created. Among these is the drivers folder, which holds the code to interact with GPIO which is what I need to do in my project/.

I am using the CMSIS in my project, 2.00.

So, I add the drivers folder to my project root, then under the quickstart panel/quick settings -> Include paths I add the path.

When I build, I get several of the following errors for each of the references to functions defined in the gpio .h/.c files. (I also add gpio.h in the C file generating the errors with "#include "gpio.h"")

Quote:
undefined reference to `GPIOSetDir'

It seems as though the .h file is found, but it can't find the functions defined in it.

Any ideas?
0 件の賞賛
返信
3 返答(返信)

890件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_USA on Fri Jul 15 15:47:29 MST 2011
You probably need to remove crp.c from the drivers folder (or tell LPCXpresso not to include it in the build) the example package with the drivers folder was created before LPCXpresso had its own CRP feature in the wizard.

-NXP
0 件の賞賛
返信

890件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Chris1seto on Thu Jul 14 19:58:28 MST 2011
Thanks,

But I still am having issues.

Now I get the following error:

Quote:
./driver/crp.o:(.crp+0x0): multiple definition of `CRP_WORD'
./src/main.o:(.crp+0x0): first defined here
c:/nxp/lpcxpresso_4.0.5_123/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -lC:/Users/Chris/Documents/LPCXpresso_4.0.5_123/workspace/MyProject/driver
c:/nxp/lpcxpresso_4.0.5_123/lpcxpresso/tools/bin/../lib/gcc/arm-none-eabi/4.5.1/../../../../arm-none-eabi/bin/ld.exe: cannot find -lC:/Users/Chris/Documents/LPCXpresso_4.0.5_123/workspace/MyProject/config
collect2: ld returned 1 exit status
make: *** [PpmEncoder.axf] Error 1



I made sure those directories exist....
0 件の賞賛
返信

890件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Jul 14 05:44:36 MST 2011
Your compiler doesn't know that you are trying to use a new source folder :eek::eek:

So just add your new source folder in:

Properties -> C/C++ General -> Paths and Symbols -> Source Location
0 件の賞賛
返信