Importing Example Projects to Win 7 to Code Red 3.6.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Importing Example Projects to Win 7 to Code Red 3.6.2

665件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by caprock on Fri Mar 25 08:31:03 MST 2011
When attempting to [B]Import Example Projects[/B] there seems to be a problem that may have something to do with the file location.

In Quick start, Click Import Examples. Then click on Browse to bring up the file chooser. Browse to C:\NXP\lpcexpresso_3.6\Examples\LPC1000\LPC17xx. Try to select any zip file (examples.lpc17xx.new.zip) and the file chooser shows [U]No items match your search.[/U] and the [I]File name:[/I] field will not populate.

But if this same file is copied to the Downloads area, then the import is successful.

Checking this file for attributes and permissions seems to be the same in either directory.

I have confirmed this behavior on my Win 7 Home Edition for both 32 & 64 bit. It feels like a Windows issue, but I can't confirm this.

Is this perhaps an Eclipse IDE or Code Red artifact?

Anyone else run into this?

:confused:
0 件の賞賛
返信
1 返信

658件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Fri Mar 25 09:52:13 MST 2011

Quote: caprock
When attempting to [B]Import Example Projects[/B] there seems to be a problem that may have something to do with the file location.
...
Anyone else run into this?

:confused:



It works fine for me on win7 pro x64.
0 件の賞賛
返信