ITM Macrocell in LPCXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ITM Macrocell in LPCXpresso IDE

1,012 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jush on Tue Feb 22 19:43:33 MST 2011
Hi,

Is LPCXpresso IDE supports ITM Macroceel for printf debugging by retargetting the ITM_SendChar() ? Just like the same way that Keil software doing.

Thanks.
0 项奖励
回复
3 回复数

986 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 23 02:33:39 MST 2011
LPCXpresso does not support use of the ITM. However, Red Suite supports a similar functionality to that provide be Keil, called Hoststrings. Note that LPC-Link does not support the ITM at all, and you need to use Red Probe+ or similar to use this functionality.
0 项奖励
回复

986 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jush on Tue Feb 22 23:11:44 MST 2011
Hello,
Ok, I see.....
Did you implement some alternative that will works like ITM Macrocell functionality?
0 项奖励
回复

986 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Feb 22 22:12:13 MST 2011
The LPCXpresso IDE does not currently use the ITM for semihosting purposes.

Regards,
CodeRedSupport
0 项奖励
回复