ITM Macrocell in LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ITM Macrocell in LPCXpresso IDE

994件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jush on Tue Feb 22 19:43:33 MST 2011
Hi,

Is LPCXpresso IDE supports ITM Macroceel for printf debugging by retargetting the ITM_SendChar() ? Just like the same way that Keil software doing.

Thanks.
0 件の賞賛
返信
3 返答(返信)

968件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Feb 23 02:33:39 MST 2011
LPCXpresso does not support use of the ITM. However, Red Suite supports a similar functionality to that provide be Keil, called Hoststrings. Note that LPC-Link does not support the ITM at all, and you need to use Red Probe+ or similar to use this functionality.
0 件の賞賛
返信

968件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jush on Tue Feb 22 23:11:44 MST 2011
Hello,
Ok, I see.....
Did you implement some alternative that will works like ITM Macrocell functionality?
0 件の賞賛
返信

968件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Feb 22 22:12:13 MST 2011
The LPCXpresso IDE does not currently use the ITM for semihosting purposes.

Regards,
CodeRedSupport
0 件の賞賛
返信