IDE question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IDE question

823件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by signumx on Tue Apr 03 08:43:33 MST 2012
Hello all,

Although it's not a big issue, is there a way to stop the IDE to automatically highlight the file in the project explorer tree when the focus is changed in the editor view.  I didn't find anything in the preferences to disable that. I dont'really like this feature as it expends the folders and the tree can get very long...

In standard Eclipse, it doesn't do that.

Thanks,
JF
0 件の賞賛
返信
2 返答(返信)

814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by signumx on Tue Apr 03 10:11:47 MST 2012
This is it!  I never really noticed that button before...

Thanks a lot!:D

JF
0 件の賞賛
返信

814件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Tue Apr 03 09:42:43 MST 2012
You tried toggling the "Link with Editor" button in the Project Explorer view?

HTH!
0 件の賞賛
返信