IDE 5.1.2 Sudden debug problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IDE 5.1.2 Sudden debug problem

782 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Apr 18 01:57:04 MST 2013
[FONT=Tahoma][SIZE=2]Suddenly, after 5 or 6 debug starts/stops (IDE continuoulsy open) I get the following error.
Error in final launch sequence
Cannot start StubMsgServer service: ImageRegistry key already in use: lpcxpresso_16x16
This is an extremely usless message for the end user (I'm sure it is clarity itself to Code Red).

So: What does this mean? I.e. why is this key in use (I checked and the debug processes are NOT still running)? How shall it be 'released'.

Obviously, I will try closing and re-opening the IDE, but I think we are entitled to an answer to this.

BTW: I have been given to understand the LPCXpresso does not use the registry.

Also, this is XP Pro/SP3.

[/SIZE][/FONT]
0 项奖励
回复
1 回复

775 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Apr 18 02:12:18 MST 2013
[FONT=Tahoma][SIZE=2]Close/open the IDE fixed the problem (whatever it was),
but I would still like to know what went wrong.
In order to  minimise the risk of it happening again.


[/SIZE][/FONT]
0 项奖励
回复