How to run LPCpresso54608

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run LPCpresso54608

1,865件の閲覧回数
実奥山
Contributor II

When  I biuld demo sample "lpcxpresso54608_demo_apps_touch_cursor" and

run(run as/run configuration/run) on MCUXpresso ,the error occured.

Comment is"" Launching lpcxpresso54608_demo_apps_touch_cursor.axf(1) has encountered a problem.

Error starting process"

Debug probe(micro B) of LPCpresso54608 board   is connected with PC in USB cable.

0 件の賞賛
返信
2 返答(返信)

1,627件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

If you are using MCUXpresso IDE, I suggest that you start off by reading the supplied User Guide which gives a good overview of importing, building and then debugging projects. If you have further issues, then I would suggest posting them to the MCUXpresso IDE forum : MCUXpresso IDE . 

For hardware / software configuration issues LPC5460x, you might also consider the LPC and the SDK forums : 

https://community.nxp.com/community/lpc 

MCUXpresso SDK 

Regards,

LPCXpresso IDE Support

0 件の賞賛
返信

1,627件の閲覧回数
実奥山
Contributor II

The above problem was settled by using "start debugging project..."

Next I tried "lpcxpress54608_demo_apps_lwip_lwip_httpsrv_bm".

I connected my borad to PC with cat5 cable.

But PC IE could not open httpserver(192.168.0.102).

Isn't the MAC address initialized?

Can I have advice?

0 件の賞賛
返信