How to read any GPIO in input state

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to read any GPIO in input state

719件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Deepak Bansal on Tue Sep 11 00:11:58 MST 2012
How to read LPC1317 in input state.I didn't find its function in gpio.c.

Also user manual do not have library description.
0 件の賞賛
返信
2 返答(返信)

706件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Deepak Bansal on Tue Sep 11 22:19:55 MST 2012
Thanks Gromak

If selected bits are required than
LPC_GPIO[portNum]->MASKED_ACCESS[bitPosi]
can be used.


regards
Deepak
0 件の賞賛
返信

706件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Tue Sep 11 06:16:41 MST 2012

Quote: Deepak Bansal
How to read LPC1317 in input state.I didn't find its function in gpio.c.

Also user manual do not have library description.



uint32_t port0_input_state;
port0_input_state=LPC_GPIO0->DATA; // reading inputs from PORT0
0 件の賞賛
返信