How to put variable at specific address with LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to put variable at specific address with LPCXpresso

2,858 Views
gregwilson-lind
Contributor II

I'm trying to build an LPC15xx bootloader and application using LPCXpresso. In the example programs the bootloader uses a signature at the end of the Flash to indicate that the Application is loaded and can be executed. I have not been able to find and example using LPCXpresso or any documentation that shows how to put the signature in the Application at the end of Flash memory.

Any pointers to documentation or LPCXpresso examples of how to locate a variable at a specific address would be greatly appreciated.

Labels (1)
Tags (1)
2 Replies

2,047 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The simplest way to validate that the flash where you are placing your application contains a real valid image would probably be to use a similar mechanism to the "valid image" word used by the ROM boot loader - basically doing a simple checksum of the first 7 words in your image, which then gets stored at 8th word in the image.

Your boot loader can then validate your image by reversing this process.

For more details, see:

Creating an LPC valid image checksum directly in the image 

LPC Image Checksums 

Otherwise, there are a variety of FAQs on placing data at specific locations, for instance:

Placing data at an address 

https://community.nxp.com/message/630738 

Regards,

LPCXpresso Support

2,047 Views
jtmiii
Contributor I

The difficulty with the checksum written into to location 0x1C is that it is weak. It assumes that image load is atomic and that it proceeded without interruption - something that cannot be assumed if IAP is used to load the application into flash from a communications link. If the goal is to ensure a highly robust and failure resistant system, a checksum of the vectors in the first block written is not sufficient. A communication failure would leave the flash with a partially written image but a valid checksum. The naive bootloader would transfer to a partially loaded image and the resulting system crash is not recoverable without a long drive, a hacked off customer, and possibly a now unemployed software engineer. (And yes, the watchdog timer may help prevent this problem, but better to avoid it entirely.)

Does LPC Support have any guidance on how to checksum the entire image at build time and then re-calculate this checksum in the bootloader so that a transfer to a defective immage will not occur (or only occur with sufficiently low probability since even a checksum will not provide certainty)?

Some thoughts that I have had, was to take another of the reserved exception vectors (likely the one at 0x28 - vector 10) and place a full image checksum there. The (custom) bootstrap loader then calculate a CRC-32 checksum across the full image, starting at location 0x2C, possibly including the unprogrammed locations to detect possible flash tampering. Using the vector at 0x28 in this manner should be safe since neither the LPC43xx parts, nor the ARM Cortex M arcitecture have a declared use for this location. 

The build process would add a few post build steps to generate the CRC-32 checksum from the project.bin file. The most likely utility is "srecord" as it is open sourced, readily available and easy to use.

The estimated computation time for this CRC-32 calculation would be sub-second for the LPC43xx flash sizes.

0 Kudos
Reply